PressureSystemParentBuilder Class¶
-
class
NXOpen.Die.
PressureSystemParentBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Pressure System Parent sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BuildStatus | Returns the build status of pressure systems. |
Clearance | Returns or sets the clearance of pressure systems. |
DesignStatus | Returns or sets the design status of pressure systems, if true the pressure systems will be built into the model, if false they will not. |
Diameter | Returns or sets the diameter of pressure systems. |
DisplayStatus | Returns or sets the display status of pressure systems, if true input data to the pressure systems will be displayed, if false the input data will not be displayed. |
Height | Returns or sets the height of pressure systems. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
XCount | Returns or sets the x count of pressure systems. |
XDistance | Returns or sets the x distance of pressure systems. |
XOffset | Returns or sets the x offset of pressure systems. |
YCount | Returns or sets the y count of pressure systems. |
YDistance | Returns or sets the y distance of pressure systems. |
YOffset | Returns or sets the y offset of pressure systems. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreateChild | Creates a child pressure system. |
DeleteChild | Deletes a child pressure system. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetChildren | Outputs the child pressure systems. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BuildStatus¶
-
PressureSystemParentBuilder.
BuildStatus
¶ Returns the build status of pressure systems.
-------------------------------------
Getter Method
Signature
BuildStatus
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Clearance¶
-
PressureSystemParentBuilder.
Clearance
¶ Returns or sets the clearance of pressure systems.
-------------------------------------
Getter Method
Signature
Clearance
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Clearance
Parameters: clearance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
PressureSystemParentBuilder.
DesignStatus
¶ Returns or sets the design status of pressure systems, if true the pressure systems will be built into the model, if false they will not.
-------------------------------------
Getter Method
Signature
DesignStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Diameter¶
-
PressureSystemParentBuilder.
Diameter
¶ Returns or sets the diameter of pressure systems.
-------------------------------------
Getter Method
Signature
Diameter
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Diameter
Parameters: diameter (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
PressureSystemParentBuilder.
DisplayStatus
¶ Returns or sets the display status of pressure systems, if true input data to the pressure systems will be displayed, if false the input data will not be displayed.
-------------------------------------
Getter Method
Signature
DisplayStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Height¶
-
PressureSystemParentBuilder.
Height
¶ Returns or sets the height of pressure systems.
-------------------------------------
Getter Method
Signature
Height
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Height
Parameters: height (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
XCount¶
-
PressureSystemParentBuilder.
XCount
¶ Returns or sets the x count of pressure systems.
-------------------------------------
Getter Method
Signature
XCount
Returns: Return type: int New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
XCount
Parameters: xCount (int) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
XDistance¶
-
PressureSystemParentBuilder.
XDistance
¶ Returns or sets the x distance of pressure systems.
-------------------------------------
Getter Method
Signature
XDistance
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
XDistance
Parameters: xDistance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
XOffset¶
-
PressureSystemParentBuilder.
XOffset
¶ Returns or sets the x offset of pressure systems.
-------------------------------------
Getter Method
Signature
XOffset
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
XOffset
Parameters: xOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
YCount¶
-
PressureSystemParentBuilder.
YCount
¶ Returns or sets the y count of pressure systems.
-------------------------------------
Getter Method
Signature
YCount
Returns: Return type: int New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
YCount
Parameters: yCount (int) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
YDistance¶
-
PressureSystemParentBuilder.
YDistance
¶ Returns or sets the y distance of pressure systems.
-------------------------------------
Getter Method
Signature
YDistance
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
YDistance
Parameters: yDistance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
YOffset¶
-
PressureSystemParentBuilder.
YOffset
¶ Returns or sets the y offset of pressure systems.
-------------------------------------
Getter Method
Signature
YOffset
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
YOffset
Parameters: yOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
CreateChild¶
-
PressureSystemParentBuilder.
CreateChild
¶ Creates a child pressure system.
Signature
CreateChild()
Returns: Return type: NXOpen.Die.PressureSystemChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DeleteChild¶
-
PressureSystemParentBuilder.
DeleteChild
¶ Deletes a child pressure system.
Signature
DeleteChild(diepressuresystemchild)
Parameters: diepressuresystemchild ( NXOpen.Die.PressureSystemChildBuilder
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetChildren¶
-
PressureSystemParentBuilder.
GetChildren
¶ Outputs the child pressure systems.
Signature
GetChildren()
Returns: The child pressure systems. Return type: list of NXOpen.Die.PressureSystemChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
PressureSystemParentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.