HoleChildBuilder Class¶
-
class
NXOpen.Die.
HoleChildBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Hole Child sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BuildStatus | Returns the build status of the die hole. |
Center | Returns or sets the center of the die hole. |
CounterBoreDiameter | Returns or sets the counter bore diameter of the die hole. |
CreateWithPad | Returns or sets the create with pad switch of the die hole, if true a pad will be created around the hole, if false the pad will not be created. |
Depth | Returns or sets the depth of the die hole. |
DesignStatus | Returns or sets the design status of the die hole, if true the hole will be built into the model, if false it will not. |
Diameter | Returns or sets the diameter of the die hole. |
DisplayHoles | Returns or sets the display holes switch of the die hole, if true the hole will be built into the model, if false it will not. |
DisplayStatus | Returns or sets the display status of the die hole, if true input data to the hole will be displayed, if false the input data will not be displayed. |
DropThruDiameter | Returns or sets the drop thru diameter of the die hole. |
PadDiameter | Returns or sets the pad diameter of the die hole. |
PadHeight | Returns or sets the pad height of the die hole. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Plane | Returns or sets the plane of the die hole. |
PlaneOffset | Returns or sets the plane offset of the die hole. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetHoleAttributes | Gets the hole attributes, note existance of attributes depends on usage in main feature. |
GetObject | Returns the object currently being edited by this builder. |
GetPadAttributes | Gets the pad attributes, note existance of attributes depends on usage in main feature. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetHoleAttributes | Sets the hole attributes, note existance of attributes depends on usage in main feature. |
SetPadAttributes | Sets the pad attributes, note existance of attributes depends on usage in main feature. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
TranslateCenter | Translates the center of the die hole by the specified amount. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BuildStatus¶
-
HoleChildBuilder.
BuildStatus
¶ Returns the build status of the die hole.
-------------------------------------
Getter Method
Signature
BuildStatus
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Center¶
-
HoleChildBuilder.
Center
¶ Returns or sets the center of the die hole.
-------------------------------------
Getter Method
Signature
Center
Returns: Return type: NXOpen.ILocation
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Center
Parameters: center ( NXOpen.ILocation
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
CounterBoreDiameter¶
-
HoleChildBuilder.
CounterBoreDiameter
¶ Returns or sets the counter bore diameter of the die hole.
-------------------------------------
Getter Method
Signature
CounterBoreDiameter
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CounterBoreDiameter
Parameters: counterBoreDiameter (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
CreateWithPad¶
-
HoleChildBuilder.
CreateWithPad
¶ Returns or sets the create with pad switch of the die hole, if true a pad will be created around the hole, if false the pad will not be created.
-------------------------------------
Getter Method
Signature
CreateWithPad
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CreateWithPad
Parameters: createWithPad (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Depth¶
-
HoleChildBuilder.
Depth
¶ Returns or sets the depth of the die hole.
-------------------------------------
Getter Method
Signature
Depth
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Depth
Parameters: depth (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
HoleChildBuilder.
DesignStatus
¶ Returns or sets the design status of the die hole, if true the hole will be built into the model, if false it will not.
-------------------------------------
Getter Method
Signature
DesignStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Diameter¶
-
HoleChildBuilder.
Diameter
¶ Returns or sets the diameter of the die hole.
-------------------------------------
Getter Method
Signature
Diameter
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Diameter
Parameters: diameter (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayHoles¶
-
HoleChildBuilder.
DisplayHoles
¶ Returns or sets the display holes switch of the die hole, if true the hole will be built into the model, if false it will not.
Note that this setting has the same affect as design status, unless the create with pad switch is true.
-------------------------------------
Getter Method
Signature
DisplayHoles
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayHoles
Parameters: displayHoles (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
HoleChildBuilder.
DisplayStatus
¶ Returns or sets the display status of the die hole, if true input data to the hole will be displayed, if false the input data will not be displayed.
-------------------------------------
Getter Method
Signature
DisplayStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DropThruDiameter¶
-
HoleChildBuilder.
DropThruDiameter
¶ Returns or sets the drop thru diameter of the die hole.
-------------------------------------
Getter Method
Signature
DropThruDiameter
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DropThruDiameter
Parameters: dropThruDiameter (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
PadDiameter¶
-
HoleChildBuilder.
PadDiameter
¶ Returns or sets the pad diameter of the die hole.
-------------------------------------
Getter Method
Signature
PadDiameter
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
PadDiameter
Parameters: padDiameter (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
PadHeight¶
-
HoleChildBuilder.
PadHeight
¶ Returns or sets the pad height of the die hole.
-------------------------------------
Getter Method
Signature
PadHeight
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
PadHeight
Parameters: padHeight (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Plane¶
-
HoleChildBuilder.
Plane
¶ Returns or sets the plane of the die hole.
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
PlaneOffset¶
-
HoleChildBuilder.
PlaneOffset
¶ Returns or sets the plane offset of the die hole.
-------------------------------------
Getter Method
Signature
PlaneOffset
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
PlaneOffset
Parameters: planeOffset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
GetHoleAttributes¶
-
HoleChildBuilder.
GetHoleAttributes
¶ Gets the hole attributes, note existance of attributes depends on usage in main feature.
Signature
GetHoleAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color, diameterTitle, depthTitle, counterBoreDiameterTitle) title is a str. Title for attribute. value is a str. Value of attribute. color is a int. Color of hole faces. diameterTitle is a str. Title for diameter attribute. depthTitle is a str. Title for depth attribute. counterBoreDiameterTitle is a str. Title for counter bore diameter attribute. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetPadAttributes¶
-
HoleChildBuilder.
GetPadAttributes
¶ Gets the pad attributes, note existance of attributes depends on usage in main feature.
Signature
GetPadAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color) title is a str. Title for attribute. value is a str. Value of attribute. color is a int. Color of pad faces. New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetHoleAttributes¶
-
HoleChildBuilder.
SetHoleAttributes
¶ Sets the hole attributes, note existance of attributes depends on usage in main feature.
Signature
SetHoleAttributes(title, value, color, diameterTitle, depthTitle, counterBoreDiameterTitle)
Parameters: - title (str) – Title for attribute.
- value (str) – Value of attribute.
- color (int) – Color of hole faces.
- diameterTitle (str) – Title for diameter attribute.
- depthTitle (str) – Title for depth attribute.
- counterBoreDiameterTitle (str) – Title for counter bore diameter attribute.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetPadAttributes¶
-
HoleChildBuilder.
SetPadAttributes
¶ Sets the pad attributes, note existance of attributes depends on usage in main feature.
Signature
SetPadAttributes(title, value, color)
Parameters: - title (str) – Title for attribute.
- value (str) – Value of attribute.
- color (int) – Color of pad faces.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
TranslateCenter¶
-
HoleChildBuilder.
TranslateCenter
¶ Translates the center of the die hole by the specified amount.
Signature
TranslateCenter(translateDist)
Parameters: translateDist ( NXOpen.Vector3d
) – A scaled vector indicating the distance to translateNew in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
HoleChildBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.