FormTaskBuilder Class¶
-
class
NXOpen.Die.
FormTaskBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Form Task feature builder.
To create a new instance of this class, use
NXOpen.Die.DieCollection.FormTask()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance of the form task. |
CamDirection | Returns or sets the cam direction of the form task. |
DistanceTolerance | Returns or sets the distance tolerance of the form task. |
FinishOperation | Returns or sets the finish operation switch of the form task, if true the form task is a finish operation, if false it is not. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PointInRegion | Returns or sets the point in region of the form task. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TippedProduct | Returns or sets the tipped product of the form task. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDetails | Gets the details of the form task. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetRegionBounds | Gets the region bounds of the form task. |
GetShapeDetail | Gets the shape detail of the form task as a profile. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetDetails | Sets the details of the form task. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetRegionBounds | Sets the region bounds of the form task. |
SetShapeDetail | Sets the shape detail of the form task using a profile. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
FormTaskBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance of the form task.
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CamDirection¶
-
FormTaskBuilder.
CamDirection
¶ Returns or sets the cam direction of the form task.
-------------------------------------
Getter Method
Signature
CamDirection
Returns: Return type: NXOpen.ILocation
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
CamDirection
Parameters: camDirection ( NXOpen.ILocation
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DistanceTolerance¶
-
FormTaskBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance of the form task.
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
FinishOperation¶
-
FormTaskBuilder.
FinishOperation
¶ Returns or sets the finish operation switch of the form task, if true the form task is a finish operation, if false it is not.
-------------------------------------
Getter Method
Signature
FinishOperation
Returns: Return type: bool New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
FinishOperation
Parameters: finishOperation (bool) – New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
PointInRegion¶
-
FormTaskBuilder.
PointInRegion
¶ Returns or sets the point in region of the form task.
-------------------------------------
Getter Method
Signature
PointInRegion
Returns: Return type: NXOpen.Point
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
PointInRegion
Parameters: pointInRegion ( NXOpen.Point
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TippedProduct¶
-
FormTaskBuilder.
TippedProduct
¶ Returns or sets the tipped product of the form task.
-------------------------------------
Getter Method
Signature
TippedProduct
Returns: Return type: NXOpen.Features.Feature
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Setter Method
Signature
TippedProduct
Parameters: tippedProduct ( NXOpen.Features.Feature
) –New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Method Detail¶
GetDetails¶
-
FormTaskBuilder.
GetDetails
¶ Gets the details of the form task.
Signature
GetDetails()
Returns: Detail strings. Return type: list of str New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetRegionBounds¶
-
FormTaskBuilder.
GetRegionBounds
¶ Gets the region bounds of the form task.
Signature
GetRegionBounds()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. The profile entries, will be curves, edges, faces, sketches or curve features. direction is aNXOpen.Die.DirectionOption
. Profile direction.New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
GetShapeDetail¶
-
FormTaskBuilder.
GetShapeDetail
¶ Gets the shape detail of the form task.
Signature
GetShapeDetail()
Returns: Sheet bodies defining the unfinished shape. Return type: list of NXOpen.Body
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetDetails¶
-
FormTaskBuilder.
SetDetails
¶ Sets the details of the form task.
Signature
SetDetails(strings)
Parameters: strings (list of str) – Detail strings. New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
SetRegionBounds¶
-
FormTaskBuilder.
SetRegionBounds
¶ Sets the region bounds of the form task.
Signature
SetRegionBounds(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
- direction (
SetShapeDetail¶
-
FormTaskBuilder.
SetShapeDetail
¶ Overloaded method SetShapeDetail
SetShapeDetail(direction, profileEntries)
SetShapeDetail(bodies)
-------------------------------------
Sets the shape detail of the form task using a profile.
Signature
SetShapeDetail(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Sets the shape detail of the form task.
Signature
SetShapeDetail(bodies)
Parameters: bodies (list of NXOpen.Body
) – Sheet bodies defining the unfinished shape.New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
-------------------------------------
Validate¶
-
FormTaskBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.