FillAreaBuilder Class¶
-
class
NXOpen.Die.
FillAreaBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder that is used to create or edit a
NXOpen.Die.FillArea
feature.To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateFillAreaBuilder()
Default values.
Property Value LowerLimitOffset.Value 1 (millimeters part), 0.04 (inches part) UpperLimitType Sheet New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance. |
BaseOrientation | Returns the plane defining the base of the target solid. |
Boundary | Returns the closed boundary profile that defines the fill area. |
DistanceTolerance | Returns or sets the distance tolerance. |
LowerLimitOffset | Returns the expression containing the lower limit offset used to adjust the lower limit to ensure a boolean. |
LowerLimitSheet | Returns the sheet (such as the inner deck sheet) used to trim the fill area solid. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Target | Returns the target solid the fill area will be united with or subtracted from. |
Type | Returns or sets the indicator for the type of fill area to build. |
UpperLimitPlane | Returns the plane used to trim the fill area solid. |
UpperLimitSheet | Returns the sheet (such as the sheet metal) used to trim the fill area solid. |
UpperLimitType | Returns or sets the value that determines whether the upper limit is defined by a sheet or plane. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FillAreaBuilderTypes Enumeration | Identifies the area of the casting the fill is targeted for. |
FillAreaBuilderUpperLimitTypes Enumeration | Specifies how the upper limit of the fill area is defined. |
Property Detail¶
AngleTolerance¶
-
FillAreaBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance.
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
BaseOrientation¶
-
FillAreaBuilder.
BaseOrientation
¶ Returns the plane defining the base of the target solid.
Used to orient the direction of the build and the trims for the fill area. May be supplied by the selected target.
-------------------------------------
Getter Method
Signature
BaseOrientation
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX7.5.0.
License requirements: None.
Boundary¶
-
FillAreaBuilder.
Boundary
¶ Returns the closed boundary profile that defines the fill area.
-------------------------------------
Getter Method
Signature
Boundary
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
DistanceTolerance¶
-
FillAreaBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
LowerLimitOffset¶
-
FillAreaBuilder.
LowerLimitOffset
¶ Returns the expression containing the lower limit offset used to adjust the lower limit to ensure a boolean.
A positive value will indicate transforming the limit away from the upper limit.
-------------------------------------
Getter Method
Signature
LowerLimitOffset
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
LowerLimitSheet¶
-
FillAreaBuilder.
LowerLimitSheet
¶ Returns the sheet (such as the inner deck sheet) used to trim the fill area solid.
This might be a sheet that is interior to the upper deck, but is always defined between the base and the upper limit. Only valid when type is
Die.FillAreaBuilderTypes.ProductContact
orDie.FillAreaBuilderTypes.UserDefined
.-------------------------------------
Getter Method
Signature
LowerLimitSheet
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
Target¶
-
FillAreaBuilder.
Target
¶ Returns the target solid the fill area will be united with or subtracted from.
-------------------------------------
Getter Method
Signature
Target
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
Type¶
-
FillAreaBuilder.
Type
¶ Returns or sets the indicator for the type of fill area to build.
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Die.FillAreaBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Die.FillAreaBuilderTypes
) –New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
UpperLimitPlane¶
-
FillAreaBuilder.
UpperLimitPlane
¶ Returns the plane used to trim the fill area solid.
A plane might be used to limit the fill area solid to just the flange of the casting. Only valid when type is
Die.FillAreaBuilderUpperLimitTypes.Plane
.-------------------------------------
Getter Method
Signature
UpperLimitPlane
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX7.5.0.
License requirements: None.
UpperLimitSheet¶
-
FillAreaBuilder.
UpperLimitSheet
¶ Returns the sheet (such as the sheet metal) used to trim the fill area solid.
Only valid when type is
Die.FillAreaBuilderUpperLimitTypes.Sheet
.-------------------------------------
Getter Method
Signature
UpperLimitSheet
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
UpperLimitType¶
-
FillAreaBuilder.
UpperLimitType
¶ Returns or sets the value that determines whether the upper limit is defined by a sheet or plane.
Only valid when type is
Die.FillAreaBuilderTypes.ScrapArea
orDie.FillAreaBuilderTypes.UserDefined
.-------------------------------------
Getter Method
Signature
UpperLimitType
Returns: Return type: NXOpen.Die.FillAreaBuilderUpperLimitTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperLimitType
Parameters: upperLimitType ( NXOpen.Die.FillAreaBuilderUpperLimitTypes
) –New in version NX7.5.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
Validate¶
-
FillAreaBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.