FillAreaBuilderUpperLimitTypes Enumeration¶
NXOpen.Die.FillAreaBuilder.UpperLimitTypes is an alias for NXOpen.Die.FillAreaBuilderUpperLimitTypes
-
class
NXOpen.Die.
FillAreaBuilderUpperLimitTypes
¶ Bases:
object
Specifies how the upper limit of the fill area is defined.
Enum Members
Enum Member Enum Member Description Sheet Upper limit is defined by a sheet body. Plane Upper limit is defined by a plane. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-