DeckParentBuilder Class¶
-
class
NXOpen.Die.
DeckParentBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Deck Feature sub feature.
Used by the Upper Draw Die and Draw Die Punch to capture the deck definition. Unless specified, the attributes and methods are generic and can be applied to any type of deck. This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BuildStatus | Returns the build status of deck. |
DesignStatus | Returns or sets the design status of deck, if true the deck will be built into the model, if false it will not. |
DisplayStatus | Returns or sets the display status of deck, if true input data to the deck will be displayed, if false the input data will not be displayed. |
InnerDeckSheet | Returns or sets the inner deck sheet of deck. |
IntermediateDeckOrientation | Returns or sets the intermediate deck orientation of the deck. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBaseFlange | Gets the base flange profile of the draw die punch. |
GetBinderEdge | Gets the binder edge profile of the upper draw die deck. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetIntermediateDeck | Gets the intermediate deck profile of the deck. |
GetMainDeck | Gets the main deck profile of the upper draw die deck. |
GetMainWallCenterline | Gets the main wall centerline profile of the draw die punch. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBaseFlange | Sets the base flange profile of the draw die punch. |
SetBinderEdge | Sets the binder edge profile of the upper draw die deck. |
SetIntermediateDeck | Sets the intermediate deck profile of the deck. |
SetMainDeck | Sets the main deck profile of the upper draw die deck. |
SetMainWallCenterline | Sets the main wall centerline profile of the draw die punch. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BuildStatus¶
-
DeckParentBuilder.
BuildStatus
¶ Returns the build status of deck.
-------------------------------------
Getter Method
Signature
BuildStatus
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
DeckParentBuilder.
DesignStatus
¶ Returns or sets the design status of deck, if true the deck will be built into the model, if false it will not.
-------------------------------------
Getter Method
Signature
DesignStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
DeckParentBuilder.
DisplayStatus
¶ Returns or sets the display status of deck, if true input data to the deck will be displayed, if false the input data will not be displayed.
-------------------------------------
Getter Method
Signature
DisplayStatus
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
InnerDeckSheet¶
-
DeckParentBuilder.
InnerDeckSheet
¶ Returns or sets the inner deck sheet of deck.
-------------------------------------
Getter Method
Signature
InnerDeckSheet
Returns: Return type: NXOpen.Body
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
InnerDeckSheet
Parameters: innerDeckSheet ( NXOpen.Body
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
IntermediateDeckOrientation¶
-
DeckParentBuilder.
IntermediateDeckOrientation
¶ Returns or sets the intermediate deck orientation of the deck.
-------------------------------------
Getter Method
Signature
IntermediateDeckOrientation
Returns: Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
IntermediateDeckOrientation
Parameters: intermediateDeckOrientation ( NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
GetBaseFlange¶
-
DeckParentBuilder.
GetBaseFlange
¶ Gets the base flange profile of the draw die punch.
Knowledge Fusion: Binder Edge of Upper Draw Die.
Signature
GetBaseFlange()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. The profile entries, will be curves, edges, faces, sketches or curve features. direction is aNXOpen.Die.DirectionOption
. Profile direction.New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetBinderEdge¶
-
DeckParentBuilder.
GetBinderEdge
¶ Gets the binder edge profile of the upper draw die deck.
Signature
GetBinderEdge()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. The profile entries, will be curves, edges, faces, sketches or curve features. direction is aNXOpen.Die.DirectionOption
. Profile direction.New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetIntermediateDeck¶
-
DeckParentBuilder.
GetIntermediateDeck
¶ Gets the intermediate deck profile of the deck.
Signature
GetIntermediateDeck()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. The profile entries, will be curves, edges, faces, sketches or curve features. direction is aNXOpen.Die.DirectionOption
. Profile direction.New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetMainDeck¶
-
DeckParentBuilder.
GetMainDeck
¶ Gets the main deck profile of the upper draw die deck.
Signature
GetMainDeck()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. The profile entries, will be curves, edges, faces, sketches or curve features. direction is aNXOpen.Die.DirectionOption
. Profile direction.New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetMainWallCenterline¶
-
DeckParentBuilder.
GetMainWallCenterline
¶ Gets the main wall centerline profile of the draw die punch.
Knowledge Fusion: Main Deck of Upper Draw Die.
Signature
GetMainWallCenterline()
Returns: a tuple Return type: A tuple consisting of (profileEntries, direction). profileEntries is a list of NXOpen.IProfile
. The profile entries, will be curves, edges, faces, sketches or curve features. direction is aNXOpen.Die.DirectionOption
. Profile direction.New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBaseFlange¶
-
DeckParentBuilder.
SetBaseFlange
¶ Sets the base flange profile of the draw die punch.
Knowledge Fusion: Binder Edge of Upper Draw Die.
Signature
SetBaseFlange(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
- direction (
SetBinderEdge¶
-
DeckParentBuilder.
SetBinderEdge
¶ Sets the binder edge profile of the upper draw die deck.
Signature
SetBinderEdge(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
- direction (
SetIntermediateDeck¶
-
DeckParentBuilder.
SetIntermediateDeck
¶ Sets the intermediate deck profile of the deck.
Signature
SetIntermediateDeck(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
- direction (
SetMainDeck¶
-
DeckParentBuilder.
SetMainDeck
¶ Sets the main deck profile of the upper draw die deck.
Signature
SetMainDeck(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
- direction (
SetMainWallCenterline¶
-
DeckParentBuilder.
SetMainWallCenterline
¶ Sets the main wall centerline profile of the draw die punch.
Knowledge Fusion: Main Deck of Upper Draw Die.
Signature
SetMainWallCenterline(direction, profileEntries)
Parameters: - direction (
NXOpen.Die.DirectionOption
) – Profile direction. - profileEntries (list of
NXOpen.IProfile
) – The profile entries, can be curves, edges, faces, sketches or curve features.
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
- direction (
Validate¶
-
DeckParentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.