ClampingSlotBuilder Class¶
-
class
NXOpen.Die.
ClampingSlotBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Clamping Slot feature builder
To create a new instance of this class, use
NXOpen.Die.DieCollection.ClampingSlot()
Default values.
Property Value CenterlineLength.Value 40 (millimeters part), 1.57 (inches part) FlangeThickness.Value 45 (millimeters part), 1.77 (inches part) InnerWidth.Value 45 (millimeters part), 1.77 (inches part) LocationOffset.Value 0 (millimeters part), 0 (inches part) LocationOnFlange false NotchAngle.Value 0 (millimeters part), 0 (inches part) NotchHeight.Value 0 (millimeters part), 0 (inches part) NotchWidth.Value 0 (millimeters part), 0 (inches part) OffsetWidth.Value 150 (millimeters part), 5.9 (inches part) Overhang.Value 0 (millimeters part), 0 (inches part) PadHeight.Value 63.5 (millimeters part), 2.5 (inches part) PadLength.Value 80 (millimeters part), 3.15 (inches part) PadOffset.Value 0 (millimeters part), 0 (inches part) PadRadius.Value 25 (millimeters part), 1.0 (inches part) PadWidth.Value 110 (millimeters part), 4.33 (inches part) SlotLength.Value 40 (millimeters part), 1.57 (inches part) SlotRadius.Value 20 (millimeters part), 0.787 (inches part) SlotWidth.Value 45 (millimeters part), 1.77 (inches part) TopLength.Value 60 (millimeters part), 2.36 (inches part) New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angle tolerance |
BasePlane | Returns the base plane of the clamping slot pad |
CenterlineLength | Returns the length from the location to the flange |
DieCenterlineCoordinateSystem | Returns the die centerline coordinate system for orienting the slot |
DistanceTolerance | Returns or sets the distance tolerance |
FlangeBaseProfile | Returns the closed profile of the flange base |
FlangeThickness | Returns the thickness of the flange |
InnerWidth | Returns the width of the cutout at the back of the slot |
LocationOffset | Returns the amount to move along the location offset direction if specified |
LocationOffsetDirection | Returns the direction to offset the clampslot locations if needed |
LocationOnFlange | Returns or sets the toggle to identify if the location should be mapped to the flange before building |
Locations | Returns the locations for the clamping slots |
NotchAngle | Returns the angle of the notch with respect to the base of the pad |
NotchFacesAttributes | Returns the attributes for the notch faces |
NotchHeight | Returns the height of the notch on the pad from the base |
NotchWidth | Returns the width from the center of the slot to the outer edge of the notch |
OffsetWidth | Returns the width of the additional flange casting added for pad support |
OrientationPlane | Returns the top orientation plane of the clamping slot pad |
Overhang | Returns the amount the pad will overhang from the flange |
OverhangFacesAttributes | Returns the attributes for the overhang faces |
PadFacesAttributes | Returns the attributes for the pad faces |
PadHeight | Returns the height of the pad |
PadLength | Returns the length of the pad from front to back |
PadOffset | Returns the amount to offset from the pad orientation to determine true top of pad |
PadRadius | Returns the radius of the pad at the back corners |
PadWidth | Returns the width of the pad |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SlotEndFacesAttributes | Returns the attributes for the end faces of the slot |
SlotFacesAttributes | Returns the attributes for the slot faces |
SlotLength | Returns the length of the slot |
SlotRadius | Returns the radius of the back cutout |
SlotWidth | Returns the width of the slot |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Target | Returns the target solid the clamp slots will be united with |
TopLength | Returns the distance from the front of the slot to the back cutout |
Type | Returns or sets the clamping slot type to build |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ClampingSlotBuilderTypes Enumeration | Clamping slot types |
Property Detail¶
AngleTolerance¶
-
ClampingSlotBuilder.
AngleTolerance
¶ Returns or sets the angle tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance
Parameters: angleTolerance (float) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
BasePlane¶
-
ClampingSlotBuilder.
BasePlane
¶ Returns the base plane of the clamping slot pad
-------------------------------------
Getter Method
Signature
BasePlane
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX6.0.0.
License requirements: None.
CenterlineLength¶
-
ClampingSlotBuilder.
CenterlineLength
¶ Returns the length from the location to the flange
-------------------------------------
Getter Method
Signature
CenterlineLength
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
DieCenterlineCoordinateSystem¶
-
ClampingSlotBuilder.
DieCenterlineCoordinateSystem
¶ Returns the die centerline coordinate system for orienting the slot
-------------------------------------
Getter Method
Signature
DieCenterlineCoordinateSystem
Returns: Return type: NXOpen.SelectCartesianCoordinateSystem
New in version NX6.0.0.
License requirements: None.
DistanceTolerance¶
-
ClampingSlotBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
FlangeBaseProfile¶
-
ClampingSlotBuilder.
FlangeBaseProfile
¶ Returns the closed profile of the flange base
-------------------------------------
Getter Method
Signature
FlangeBaseProfile
Returns: Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
FlangeThickness¶
-
ClampingSlotBuilder.
FlangeThickness
¶ Returns the thickness of the flange
-------------------------------------
Getter Method
Signature
FlangeThickness
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
InnerWidth¶
-
ClampingSlotBuilder.
InnerWidth
¶ Returns the width of the cutout at the back of the slot
-------------------------------------
Getter Method
Signature
InnerWidth
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
LocationOffset¶
-
ClampingSlotBuilder.
LocationOffset
¶ Returns the amount to move along the location offset direction if specified
-------------------------------------
Getter Method
Signature
LocationOffset
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
LocationOffsetDirection¶
-
ClampingSlotBuilder.
LocationOffsetDirection
¶ Returns the direction to offset the clampslot locations if needed
-------------------------------------
Getter Method
Signature
LocationOffsetDirection
Returns: Return type: NXOpen.Die.DieDirectionBuilder
New in version NX6.0.0.
License requirements: None.
LocationOnFlange¶
-
ClampingSlotBuilder.
LocationOnFlange
¶ Returns or sets the toggle to identify if the location should be mapped to the flange before building
-------------------------------------
Getter Method
Signature
LocationOnFlange
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocationOnFlange
Parameters: locationOnFlange (bool) – New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
Locations¶
-
ClampingSlotBuilder.
Locations
¶ Returns the locations for the clamping slots
-------------------------------------
Getter Method
Signature
Locations
Returns: Return type: NXOpen.Die.DieLocationsBuilder
New in version NX6.0.0.
License requirements: None.
NotchAngle¶
-
ClampingSlotBuilder.
NotchAngle
¶ Returns the angle of the notch with respect to the base of the pad
-------------------------------------
Getter Method
Signature
NotchAngle
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
NotchFacesAttributes¶
-
ClampingSlotBuilder.
NotchFacesAttributes
¶ Returns the attributes for the notch faces
-------------------------------------
Getter Method
Signature
NotchFacesAttributes
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
NotchHeight¶
-
ClampingSlotBuilder.
NotchHeight
¶ Returns the height of the notch on the pad from the base
-------------------------------------
Getter Method
Signature
NotchHeight
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
NotchWidth¶
-
ClampingSlotBuilder.
NotchWidth
¶ Returns the width from the center of the slot to the outer edge of the notch
-------------------------------------
Getter Method
Signature
NotchWidth
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
OffsetWidth¶
-
ClampingSlotBuilder.
OffsetWidth
¶ Returns the width of the additional flange casting added for pad support
-------------------------------------
Getter Method
Signature
OffsetWidth
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
OrientationPlane¶
-
ClampingSlotBuilder.
OrientationPlane
¶ Returns the top orientation plane of the clamping slot pad
-------------------------------------
Getter Method
Signature
OrientationPlane
Returns: Return type: NXOpen.Die.DiePlaneBuilder
New in version NX6.0.0.
License requirements: None.
Overhang¶
-
ClampingSlotBuilder.
Overhang
¶ Returns the amount the pad will overhang from the flange
-------------------------------------
Getter Method
Signature
Overhang
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
OverhangFacesAttributes¶
-
ClampingSlotBuilder.
OverhangFacesAttributes
¶ Returns the attributes for the overhang faces
-------------------------------------
Getter Method
Signature
OverhangFacesAttributes
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
PadFacesAttributes¶
-
ClampingSlotBuilder.
PadFacesAttributes
¶ Returns the attributes for the pad faces
-------------------------------------
Getter Method
Signature
PadFacesAttributes
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
PadHeight¶
-
ClampingSlotBuilder.
PadHeight
¶ Returns the height of the pad
-------------------------------------
Getter Method
Signature
PadHeight
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PadLength¶
-
ClampingSlotBuilder.
PadLength
¶ Returns the length of the pad from front to back
-------------------------------------
Getter Method
Signature
PadLength
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PadOffset¶
-
ClampingSlotBuilder.
PadOffset
¶ Returns the amount to offset from the pad orientation to determine true top of pad
-------------------------------------
Getter Method
Signature
PadOffset
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PadRadius¶
-
ClampingSlotBuilder.
PadRadius
¶ Returns the radius of the pad at the back corners
-------------------------------------
Getter Method
Signature
PadRadius
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PadWidth¶
-
ClampingSlotBuilder.
PadWidth
¶ Returns the width of the pad
-------------------------------------
Getter Method
Signature
PadWidth
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SlotEndFacesAttributes¶
-
ClampingSlotBuilder.
SlotEndFacesAttributes
¶ Returns the attributes for the end faces of the slot
-------------------------------------
Getter Method
Signature
SlotEndFacesAttributes
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
SlotFacesAttributes¶
-
ClampingSlotBuilder.
SlotFacesAttributes
¶ Returns the attributes for the slot faces
-------------------------------------
Getter Method
Signature
SlotFacesAttributes
Returns: Return type: NXOpen.Die.DieAttributesBuilder
New in version NX6.0.0.
License requirements: None.
SlotLength¶
-
ClampingSlotBuilder.
SlotLength
¶ Returns the length of the slot
-------------------------------------
Getter Method
Signature
SlotLength
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SlotRadius¶
-
ClampingSlotBuilder.
SlotRadius
¶ Returns the radius of the back cutout
-------------------------------------
Getter Method
Signature
SlotRadius
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
SlotWidth¶
-
ClampingSlotBuilder.
SlotWidth
¶ Returns the width of the slot
-------------------------------------
Getter Method
Signature
SlotWidth
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Target¶
-
ClampingSlotBuilder.
Target
¶ Returns the target solid the clamp slots will be united with
-------------------------------------
Getter Method
Signature
Target
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
TopLength¶
-
ClampingSlotBuilder.
TopLength
¶ Returns the distance from the front of the slot to the back cutout
-------------------------------------
Getter Method
Signature
TopLength
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Type¶
-
ClampingSlotBuilder.
Type
¶ Returns or sets the clamping slot type to build
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Die.ClampingSlotBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Die.ClampingSlotBuilderTypes
) –New in version NX6.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
Validate¶
-
ClampingSlotBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.