DieLocationsBuilder Class¶
-
class
NXOpen.Die.
DieLocationsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Die.DieLocationsBuilder
.The Die Locations is a helper to the main Die Design feature to gather the location points for items such as hole center or clamping slot location. Note that a non-point is selected, such as a plane or coordinate system, the control point of the object will be used for the location.
To create a new instance of this class, use
NXOpen.Die.DieCollection.CreateDieLocations()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
List | Returns the list containing the die location objects |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
List¶
-
DieLocationsBuilder.
List
¶ Returns the list containing the die location objects
-------------------------------------
Getter Method
Signature
List
Returns: Return type: NXOpen.Die.DieLocationBuilderList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
DieLocationsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.