LineTypeBuilder Class¶
-
class
NXOpen.DiagrammingLibraryAuthor.
LineTypeBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a LineTypeBuilder.
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
LineColor | Returns or sets the line color. |
LineFont | Returns or sets the line font. |
LineTypeName | Returns or sets the name of the line type. |
LineTypePriority | Returns or sets the priority of the line type. |
LineWidth | Returns or sets the line width. |
ObjectId | Returns the object Id of the line type. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LineColor¶
-
LineTypeBuilder.
LineColor
¶ Returns or sets the line color.
-------------------------------------
Getter Method
Signature
LineColor
Returns: Return type: Id New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineColor
Parameters: colorId (Id) – New in version NX11.0.1.
License requirements: None.
LineFont¶
-
LineTypeBuilder.
LineFont
¶ Returns or sets the line font.
-------------------------------------
Getter Method
Signature
LineFont
Returns: Return type: NXOpen.DisplayableObjectObjectFont
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineFont
Parameters: font ( NXOpen.DisplayableObjectObjectFont
) –New in version NX11.0.1.
License requirements: None.
LineTypeName¶
-
LineTypeBuilder.
LineTypeName
¶ Returns or sets the name of the line type.
It should be unique.
-------------------------------------
Getter Method
Signature
LineTypeName
Returns: Return type: str New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineTypeName
Parameters: name (str) – New in version NX11.0.1.
License requirements: None.
LineTypePriority¶
-
LineTypeBuilder.
LineTypePriority
¶ Returns or sets the priority of the line type.
It should be greater than or equal to 0.
-------------------------------------
Getter Method
Signature
LineTypePriority
Returns: Return type: int New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineTypePriority
Parameters: priority (int) – New in version NX11.0.1.
License requirements: None.
LineWidth¶
-
LineTypeBuilder.
LineWidth
¶ Returns or sets the line width.
-------------------------------------
Getter Method
Signature
LineWidth
Returns: Return type: NXOpen.DisplayableObjectObjectWidth
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineWidth
Parameters: width ( NXOpen.DisplayableObjectObjectWidth
) –New in version NX11.0.1.
License requirements: None.
Method Detail¶
Validate¶
-
LineTypeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.