TurnGrooveCornerControl Class¶
-
class
NXOpen.CAM.
TurnGrooveCornerControl
¶ Bases:
NXOpen.TaggedObject
Represents a groove corner control ja
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CornerType | Returns or sets the Groove Corner Control corner type |
CutSequence | Returns or sets the Groove Corner Control cut sequence |
RadiusOrDistance | Returns or sets the Groove Corner Control radius or distance |
ReliefPlungeDistance | Returns or sets the Groove Corner Control relief plunge distance |
ReliefPlungeOffset | Returns or sets the Groove Corner Control relief plunge offset |
ReliefPlungeType | Returns or sets the Groove Corner Control relief plunge type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TurnGrooveCornerControlCornerTypes Enumeration | the Groove Corner Control corner types |
TurnGrooveCornerControlCutSequenceTypes Enumeration | the Groove Corner Control cut sequence types |
TurnGrooveCornerControlReliefPlungeTypes Enumeration | the Groove Corner Control relief plunge types |
Property Detail¶
CornerType¶
-
TurnGrooveCornerControl.
CornerType
¶ Returns or sets the Groove Corner Control corner type
-------------------------------------
Getter Method
Signature
CornerType
Returns: the Groove Corner Control corner type Return type: NXOpen.CAM.TurnGrooveCornerControlCornerTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerType
Parameters: cornerType ( NXOpen.CAM.TurnGrooveCornerControlCornerTypes
) – the Groove Corner Control corner typeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
CutSequence¶
-
TurnGrooveCornerControl.
CutSequence
¶ Returns or sets the Groove Corner Control cut sequence
-------------------------------------
Getter Method
Signature
CutSequence
Returns: the Groove Corner Control cut sequence Return type: NXOpen.CAM.TurnGrooveCornerControlCutSequenceTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutSequence
Parameters: cutSequence ( NXOpen.CAM.TurnGrooveCornerControlCutSequenceTypes
) – the Groove Corner Control cut sequenceNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
RadiusOrDistance¶
-
TurnGrooveCornerControl.
RadiusOrDistance
¶ Returns or sets the Groove Corner Control radius or distance
-------------------------------------
Getter Method
Signature
RadiusOrDistance
Returns: the Groove Corner Control radius or distance Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadiusOrDistance
Parameters: radiusOrDistance (float) – the Groove Corner Control radius or distance New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
ReliefPlungeDistance¶
-
TurnGrooveCornerControl.
ReliefPlungeDistance
¶ Returns or sets the Groove Corner Control relief plunge distance
-------------------------------------
Getter Method
Signature
ReliefPlungeDistance
Returns: the Groove Corner Control relief plunge distance Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReliefPlungeDistance
Parameters: reliefPlungeDistance (float) – the Groove Corner Control relief plunge distance New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
ReliefPlungeOffset¶
-
TurnGrooveCornerControl.
ReliefPlungeOffset
¶ Returns or sets the Groove Corner Control relief plunge offset
-------------------------------------
Getter Method
Signature
ReliefPlungeOffset
Returns: the Groove Corner Control relief plunge offset Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReliefPlungeOffset
Parameters: reliefPlungeOffset (float) – the Groove Corner Control relief plunge offset New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
ReliefPlungeType¶
-
TurnGrooveCornerControl.
ReliefPlungeType
¶ Returns or sets the Groove Corner Control relief plunge type
-------------------------------------
Getter Method
Signature
ReliefPlungeType
Returns: the Groove Corner Control relief plunge type Return type: NXOpen.CAM.TurnGrooveCornerControlReliefPlungeTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReliefPlungeType
Parameters: reliefPlungeType ( NXOpen.CAM.TurnGrooveCornerControlReliefPlungeTypes
) – the Groove Corner Control relief plunge typeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)