TurnGrooveCornerControlCornerTypes Enumeration¶
NXOpen.CAM.TurnGrooveCornerControl.CornerTypes is an alias for NXOpen.CAM.TurnGrooveCornerControlCornerTypes
-
class
NXOpen.CAM.
TurnGrooveCornerControlCornerTypes
¶ Bases:
object
the Groove Corner Control corner types
New in version NX9.0.0.
Enum Members
Enum Member Enum Member Description NotSet Groove Corner Control corner type is None. FollowPart Groove Corner Control corner type is Follow Part. Round Groove Corner Control corner type is Round. Break Groove Corner Control corner type is Break. RoundIpw Groove Corner Control corner type is Round (IPW). BreakIpw Groove Corner Control corner type is Break (IPW). -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-