TurnGrooveCornerControlCutSequenceTypes Enumeration¶
NXOpen.CAM.TurnGrooveCornerControl.CutSequenceTypes is an alias for NXOpen.CAM.TurnGrooveCornerControlCutSequenceTypes
-
class
NXOpen.CAM.
TurnGrooveCornerControlCutSequenceTypes
¶ Bases:
object
the Groove Corner Control cut sequence types
New in version NX9.0.0.
Enum Members
Enum Member Enum Member Description CornersFirst Groove Corner Control cut sequence is Corners First. CornersFirstAndLast Groove Corner Control cut sequence is Corners First and Last. CornerWithWall Groove Corner Control cut sequence is Corner With Wall. CornerAfterWall Groove Corner Control cut sequence is Corner After Wall. CornersLast Groove Corner Control cut sequence is Corners Last. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-