Properties¶
Property | Description |
---|---|
AvoidanceApproachBuilder | Returns the approach path builder |
AvoidanceClearanceBuilder | Returns the clearance builder |
AvoidanceDepartureBuilder | Returns the departure path builder |
AvoidanceFromBuilder | Returns the avoidance from builder |
AvoidanceGohomeBuilder | Returns the gohome point builder |
AvoidanceReturnBuilder | Returns the return path builder |
AvoidanceStartBuilder | Returns the start point builder |
AvoidanceStartOfEngageBuilder | Returns the start of engage builder |
BlankOffsetBuilder | Returns the blank offset (inheritable double) |
CheckOffsetBuilder | Returns the check offset (inheritable double) |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
GeometryCiBuilder | Returns the geometry builder |
LayoutCiBuilder | Returns the save/layer layout builder |
OptimizationMethod | Returns or sets the optim method |
PartMaterialBuilder | Returns or sets the part material |
PartOffsetBuilder | Returns the part offset (inheritable double) |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TrimOffsetBuilder | Returns the trim offset (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetMaterial | Get part material |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetMaterial | Set part material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AvoidanceApproachBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceApproachBuilder
¶ Returns the approach path builder
-------------------------------------
Getter Method
Signature
AvoidanceApproachBuilder
Returns: the avoidance approach builder Return type: NXOpen.CAM.TurnAvoidanceApproachBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceClearanceBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceClearanceBuilder
¶ Returns the clearance builder
-------------------------------------
Getter Method
Signature
AvoidanceClearanceBuilder
Returns: the avoidance clearance builder Return type: NXOpen.CAM.TurnAvoidanceClearanceBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceDepartureBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceDepartureBuilder
¶ Returns the departure path builder
-------------------------------------
Getter Method
Signature
AvoidanceDepartureBuilder
Returns: the avoidance departure path builder Return type: NXOpen.CAM.TurnAvoidanceDepartureBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceFromBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceFromBuilder
¶ Returns the avoidance from builder
-------------------------------------
Getter Method
Signature
AvoidanceFromBuilder
Returns: the avoidance from builder Return type: NXOpen.CAM.TurnAvoidanceFromBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceGohomeBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceGohomeBuilder
¶ Returns the gohome point builder
-------------------------------------
Getter Method
Signature
AvoidanceGohomeBuilder
Returns: the avoidance gohome path builder Return type: NXOpen.CAM.TurnAvoidanceGohomeBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceReturnBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceReturnBuilder
¶ Returns the return path builder
-------------------------------------
Getter Method
Signature
AvoidanceReturnBuilder
Returns: the avoidance return path builder Return type: NXOpen.CAM.TurnAvoidanceReturnBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceStartBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceStartBuilder
¶ Returns the start point builder
-------------------------------------
Getter Method
Signature
AvoidanceStartBuilder
Returns: the avoidance start builder Return type: NXOpen.CAM.TurnAvoidanceStartBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
AvoidanceStartOfEngageBuilder¶
-
TurnAvoidanceGeomBuilder.
AvoidanceStartOfEngageBuilder
¶ Returns the start of engage builder
-------------------------------------
Getter Method
Signature
AvoidanceStartOfEngageBuilder
Returns: the avoidance start of engage builder Return type: NXOpen.CAM.TurnAvoidanceStartOfEngageBuilder
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
TurnAvoidanceGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.