Properties¶
Property | Description |
---|---|
StartOfEngageMotionType | Returns or sets the start of engage motion type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TurnAvoidanceStartOfEngageBuilderStartOfEngageMotionTypes Enumeration | The start of engage motion type options |
Property Detail¶
StartOfEngageMotionType¶
-
TurnAvoidanceStartOfEngageBuilder.
StartOfEngageMotionType
¶ Returns or sets the start of engage motion type
-------------------------------------
Getter Method
Signature
StartOfEngageMotionType
Returns: the start of engage motion type value Return type: NXOpen.CAM.TurnAvoidanceStartOfEngageBuilderStartOfEngageMotionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartOfEngageMotionType
Parameters: startOfEngageMotionType ( NXOpen.CAM.TurnAvoidanceStartOfEngageBuilderStartOfEngageMotionTypes
) – the start of engage motion type valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)