TurnAvoidanceStartOfEngageBuilderStartOfEngageMotionTypes Enumeration¶
NXOpen.CAM.TurnAvoidanceStartOfEngageBuilder.StartOfEngageMotionTypes is an alias for NXOpen.CAM.TurnAvoidanceStartOfEngageBuilderStartOfEngageMotionTypes
-
class
NXOpen.CAM.
TurnAvoidanceStartOfEngageBuilderStartOfEngageMotionTypes
¶ Bases:
object
The start of engage motion type options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description Automatic Motion type: Automatic to start of engage. Direct Motion type: Direct to start of engage. RadialThenAxial Motion type: Radial then axial to start of engage. AxialThenRadial Motion type: Axial then radial to start of engage. ClearRadialThenDirect Motion type: Radial to clearance plane then direct to start of engage. ClearAxialThenDirect Motion type: Axial to clearance plane then direct to start of engage. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-