ThreadTurningBuilder Class¶
-
class
NXOpen.CAM.
ThreadTurningBuilder
¶ Bases:
NXOpen.CAM.TurningOperationBuilder
Represents a ThreadTurning Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateThreadTurningBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AdditionalCommands | Returns or sets the Additional Commands |
ChannelName | Returns or sets the channel’s name |
CrestLine | Returns or sets the Crest Line |
CrestLineDirection | Returns or sets the Crest Line Direction(Start and End Points) |
CrestOffset | Returns the crest offset builder |
CutParameters | Returns the cut parameter object |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
DepthOption | Returns or sets the depth option |
Description | Returns or sets the description |
EndLine | Returns or sets the End Line |
EndOfPath | Returns the end event builder |
EndOffset | Returns the End Offset |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds and speeds builder |
FlipToolAroundHolder | Returns or sets the Flip Tool Around Holder toggle |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
InfeedLength | Returns the infeed length |
InfeedLengthType | Returns or sets the infeed length type |
InfeedMode | Returns or sets the infeed mode |
InfeedMoveAngle | Returns the infeed move angle |
InfeedStartLineAngle | Returns the infeed start line angle |
LayoutAndLayer | Returns the Layer and Layout |
MachineCycleSubroutineName | Returns or sets the machine cycle subroutine name |
MotionOutput | Returns or sets the motion output |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ReorientToolHolder | Returns or sets the Reorient Tool Holder toggle. |
ReorientToolHolderMode | Returns or sets the Reorient Tool Holder Mode |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RootLine | Returns or sets the Root Line |
RootOffset | Returns the root offset |
RotateTrackingPoint | Returns or sets the Rotate Tracking Point toggle |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartOffset | Returns the Start Offset |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ThreadAngleBuilder | Returns the thread angle |
ToolChangeSetting | Returns the tool change builder |
ToolHolderAngle | Returns the Tool Holder Angle |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
TotalDepth | Returns the Total Depth |
TrackingPointStatus | Returns or sets the tracking point status |
UpdateIpw | Returns or sets the update IPW mode |
UseMachineCycle | Returns or sets the Use Machine Cycle toggle |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ThreadTurningBuilderDepthOptionTypes Enumeration | the Depth Option types |
ThreadTurningBuilderInfeedLengthTypes Enumeration | the Infeed Length Types |
ThreadTurningBuilderInfeedModes Enumeration | the Infeed modes |
Property Detail¶
CrestLine¶
-
ThreadTurningBuilder.
CrestLine
¶ Returns or sets the Crest Line
-------------------------------------
Getter Method
Signature
CrestLine
Returns: the Crest Line tag Return type: NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrestLine
Parameters: crestLine ( NXOpen.NXObject
) – the Crest Line tagNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CrestLineDirection¶
-
ThreadTurningBuilder.
CrestLineDirection
¶ Returns or sets the Crest Line Direction(Start and End Points)
-------------------------------------
Getter Method
Signature
CrestLineDirection
Returns: the Crest Line Direction tag Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrestLineDirection
Parameters: crestLineDirection (bool) – the Crest Line Direction tag New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
CrestOffset¶
-
ThreadTurningBuilder.
CrestOffset
¶ Returns the crest offset builder
-------------------------------------
Getter Method
Signature
CrestOffset
Returns: the crest offset Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
CutParameters¶
-
ThreadTurningBuilder.
CutParameters
¶ Returns the cut parameter object
-------------------------------------
Getter Method
Signature
CutParameters
Returns: Return type: NXOpen.CAM.ThreadCutParameters
New in version NX6.0.0.
License requirements: None.
DepthOption¶
-
ThreadTurningBuilder.
DepthOption
¶ Returns or sets the depth option
-------------------------------------
Getter Method
Signature
DepthOption
Returns: the depth option Return type: NXOpen.CAM.ThreadTurningBuilderDepthOptionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthOption
Parameters: depthOption ( NXOpen.CAM.ThreadTurningBuilderDepthOptionTypes
) – the depth optionNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
EndLine¶
-
ThreadTurningBuilder.
EndLine
¶ Returns or sets the End Line
-------------------------------------
Getter Method
Signature
EndLine
Returns: the End Line Return type: NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndLine
Parameters: endLine ( NXOpen.NXObject
) – the End Line tagNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
EndOffset¶
-
ThreadTurningBuilder.
EndOffset
¶ Returns the End Offset
-------------------------------------
Getter Method
Signature
EndOffset
Returns: the end offset Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
InfeedLength¶
-
ThreadTurningBuilder.
InfeedLength
¶ Returns the infeed length
-------------------------------------
Getter Method
Signature
InfeedLength
Returns: the infeed length Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
InfeedLengthType¶
-
ThreadTurningBuilder.
InfeedLengthType
¶ Returns or sets the infeed length type
-------------------------------------
Getter Method
Signature
InfeedLengthType
Returns: the infeed length type Return type: NXOpen.CAM.ThreadTurningBuilderInfeedLengthTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InfeedLengthType
Parameters: infeedLengthType ( NXOpen.CAM.ThreadTurningBuilderInfeedLengthTypes
) – the infeed length typeNew in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
InfeedMode¶
-
ThreadTurningBuilder.
InfeedMode
¶ Returns or sets the infeed mode
-------------------------------------
Getter Method
Signature
InfeedMode
Returns: the infeed mode Return type: NXOpen.CAM.ThreadTurningBuilderInfeedModes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InfeedMode
Parameters: infeedMode ( NXOpen.CAM.ThreadTurningBuilderInfeedModes
) – the infeed modeNew in version NX8.5.0.
License requirements: cam_base (“CAM BASE”)
InfeedMoveAngle¶
-
ThreadTurningBuilder.
InfeedMoveAngle
¶ Returns the infeed move angle
-------------------------------------
Getter Method
Signature
InfeedMoveAngle
Returns: the infeed move angle Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
InfeedStartLineAngle¶
-
ThreadTurningBuilder.
InfeedStartLineAngle
¶ Returns the infeed start line angle
-------------------------------------
Getter Method
Signature
InfeedStartLineAngle
Returns: the infeed start line angle Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
NonCuttingBuilder¶
-
ThreadTurningBuilder.
NonCuttingBuilder
¶ Returns the non-cutting builder
-------------------------------------
Getter Method
Signature
NonCuttingBuilder
Returns: the non-cutting builder Return type: NXOpen.CAM.NcmTurnThreadBuilder
New in version NX6.0.0.
License requirements: None.
RootLine¶
-
ThreadTurningBuilder.
RootLine
¶ Returns or sets the Root Line
-------------------------------------
Getter Method
Signature
RootLine
Returns: the Root Line tag Return type: NXOpen.NXObject
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RootLine
Parameters: rootLine ( NXOpen.NXObject
) – the Root Line tagNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RootOffset¶
-
ThreadTurningBuilder.
RootOffset
¶ Returns the root offset
-------------------------------------
Getter Method
Signature
RootOffset
Returns: the root offset Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
StartOffset¶
-
ThreadTurningBuilder.
StartOffset
¶ Returns the Start Offset
-------------------------------------
Getter Method
Signature
StartOffset
Returns: the start offset Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
ThreadAngleBuilder¶
-
ThreadTurningBuilder.
ThreadAngleBuilder
¶ Returns the thread angle
-------------------------------------
Getter Method
Signature
ThreadAngleBuilder
Returns: the thread angle Return type: NXOpen.CAM.CutAngle
New in version NX7.5.0.
License requirements: None.
TotalDepth¶
-
ThreadTurningBuilder.
TotalDepth
¶ Returns the Total Depth
-------------------------------------
Getter Method
Signature
TotalDepth
Returns: the total depth Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ThreadTurningBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.