ProbeInspectSurfacePointMoveBuilder Class¶
-
class
NXOpen.CAM.
ProbeInspectSurfacePointMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents the Probe Inspect Surface Point Move Builder
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateProbeInspectSurfacePointMoveBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DirectionType | Returns or sets the direction type |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
MeasurementType | Returns or sets the measurement (axis) type |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
Point | Returns or sets the point to probe |
ProbeControlParameters | Returns the probe control parameters builder |
ProbeProtectedParameters | Returns the probe protected parameters builder |
ProbeStockParameters | Returns the probe stock parameters builder |
ProbeToleranceParameters | Returns the probe tolerance parameters builder |
ProtectedMove | Returns or sets the protected move status |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
ToolAxisType | Returns or sets the probe axis type |
Vector | Returns or sets the vector to define probing direction |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProbeInspectSurfacePointMoveBuilderDirection Enumeration | the probing direction type |
ProbeInspectSurfacePointMoveBuilderMeasurement Enumeration | the measurement type |
ProbeInspectSurfacePointMoveBuilderToolAxis Enumeration | the probing tool axis type |
Property Detail¶
DirectionType¶
-
ProbeInspectSurfacePointMoveBuilder.
DirectionType
¶ Returns or sets the direction type
-------------------------------------
Getter Method
Signature
DirectionType
Returns: Return type: NXOpen.CAM.ProbeInspectSurfacePointMoveBuilderDirection
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionType
Parameters: dirType ( NXOpen.CAM.ProbeInspectSurfacePointMoveBuilderDirection
) –New in version NX5.0.0.
License requirements: None.
MeasurementType¶
-
ProbeInspectSurfacePointMoveBuilder.
MeasurementType
¶ Returns or sets the measurement (axis) type
-------------------------------------
Getter Method
Signature
MeasurementType
Returns: Return type: NXOpen.CAM.ProbeInspectSurfacePointMoveBuilderMeasurement
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MeasurementType
Parameters: measType ( NXOpen.CAM.ProbeInspectSurfacePointMoveBuilderMeasurement
) –New in version NX5.0.0.
License requirements: None.
Point¶
-
ProbeInspectSurfacePointMoveBuilder.
Point
¶ Returns or sets the point to probe
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: point ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: None.
ProbeControlParameters¶
-
ProbeInspectSurfacePointMoveBuilder.
ProbeControlParameters
¶ Returns the probe control parameters builder
-------------------------------------
Getter Method
Signature
ProbeControlParameters
Returns: Return type: NXOpen.CAM.ProbeControlParametersBuilder
New in version NX5.0.0.
License requirements: None.
ProbeProtectedParameters¶
-
ProbeInspectSurfacePointMoveBuilder.
ProbeProtectedParameters
¶ Returns the probe protected parameters builder
-------------------------------------
Getter Method
Signature
ProbeProtectedParameters
Returns: Return type: NXOpen.CAM.ProbeProtectedParametersBuilder
New in version NX5.0.0.
License requirements: None.
ProbeStockParameters¶
-
ProbeInspectSurfacePointMoveBuilder.
ProbeStockParameters
¶ Returns the probe stock parameters builder
-------------------------------------
Getter Method
Signature
ProbeStockParameters
Returns: Return type: NXOpen.CAM.ProbeStockParametersBuilder
New in version NX5.0.0.
License requirements: None.
ProbeToleranceParameters¶
-
ProbeInspectSurfacePointMoveBuilder.
ProbeToleranceParameters
¶ Returns the probe tolerance parameters builder
-------------------------------------
Getter Method
Signature
ProbeToleranceParameters
Returns: Return type: NXOpen.CAM.ProbeToleranceParametersBuilder
New in version NX5.0.0.
License requirements: None.
ToolAxisType¶
-
ProbeInspectSurfacePointMoveBuilder.
ToolAxisType
¶ Returns or sets the probe axis type
-------------------------------------
Getter Method
Signature
ToolAxisType
Returns: Return type: NXOpen.CAM.ProbeInspectSurfacePointMoveBuilderToolAxis
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolAxisType
Parameters: axisType ( NXOpen.CAM.ProbeInspectSurfacePointMoveBuilderToolAxis
) –New in version NX7.5.0.
License requirements: None.
Vector¶
-
ProbeInspectSurfacePointMoveBuilder.
Vector
¶ Returns or sets the vector to define probing direction
-------------------------------------
Getter Method
Signature
Vector
Returns: Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector
Parameters: vector ( NXOpen.NXObject
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ProbeInspectSurfacePointMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.