ProbeProtectedParametersBuilder Class¶
-
class
NXOpen.CAM.
ProbeProtectedParametersBuilder
¶ Bases:
NXOpen.TaggedObject
Represents the Probe Protected Parameters Builder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ApproachFlag | Returns or sets the approach from clearance plane flag |
ClearanceDistance | Returns or sets the safe clearance distance for external features |
CollisionFlag | Returns or sets the collision flag |
ReturnFlag | Returns or sets the return to clearance plane flag |
StandoffDistance | Returns or sets the standoff distance |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
ProbeProtectedParametersBuilderAppMethodTypes Enumeration | the approach types |
ProbeProtectedParametersBuilderCollisionFlagTypes Enumeration | the collision flag types |
ProbeProtectedParametersBuilderDepMethodTypes Enumeration | the departure types |
Property Detail¶
ApproachFlag¶
-
ProbeProtectedParametersBuilder.
ApproachFlag
¶ Returns or sets the approach from clearance plane flag
-------------------------------------
Getter Method
Signature
ApproachFlag
Returns: Return type: NXOpen.CAM.ProbeProtectedParametersBuilderAppMethodTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApproachFlag
Parameters: approachFrom ( NXOpen.CAM.ProbeProtectedParametersBuilderAppMethodTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ClearanceDistance¶
-
ProbeProtectedParametersBuilder.
ClearanceDistance
¶ Returns or sets the safe clearance distance for external features
-------------------------------------
Getter Method
Signature
ClearanceDistance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceDistance
Parameters: clearanceDistance (float) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CollisionFlag¶
-
ProbeProtectedParametersBuilder.
CollisionFlag
¶ Returns or sets the collision flag
-------------------------------------
Getter Method
Signature
CollisionFlag
Returns: Return type: NXOpen.CAM.ProbeProtectedParametersBuilderCollisionFlagTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollisionFlag
Parameters: collFlag ( NXOpen.CAM.ProbeProtectedParametersBuilderCollisionFlagTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ReturnFlag¶
-
ProbeProtectedParametersBuilder.
ReturnFlag
¶ Returns or sets the return to clearance plane flag
-------------------------------------
Getter Method
Signature
ReturnFlag
Returns: Return type: NXOpen.CAM.ProbeProtectedParametersBuilderDepMethodTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReturnFlag
Parameters: returnTo ( NXOpen.CAM.ProbeProtectedParametersBuilderDepMethodTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
StandoffDistance¶
-
ProbeProtectedParametersBuilder.
StandoffDistance
¶ Returns or sets the standoff distance
-------------------------------------
Getter Method
Signature
StandoffDistance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StandoffDistance
Parameters: standoffDistance (float) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)