ProbeProtectedParametersBuilderAppMethodTypes Enumeration¶
NXOpen.CAM.ProbeProtectedParametersBuilder.AppMethodTypes is an alias for NXOpen.CAM.ProbeProtectedParametersBuilderAppMethodTypes
-
class
NXOpen.CAM.
ProbeProtectedParametersBuilderAppMethodTypes
¶ Bases:
object
the approach types
Enum Members
Enum Member Enum Member Description NotSet none Clearance from/to clearance Direct direct RadialAxial radial and then axial AxialRadial axial and then radial RadialAxialWithClearance radial and then axial from/to clearance AxialRadialWithClearance axial and then radial from/to clearance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-