Preferences Class¶
-
class
NXOpen.CAM.
Preferences
¶ Bases:
NXOpen.Builder
Represents a cam preferences Builder
To create a new instance of this class, use
NXOpen.CAM.CAMSession.CreateCamPreferences()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AlwaysUpdateDialogs | Returns or sets the auto update dialog |
AutomaticallySetMachingData | Returns or sets the auto maching data |
AuxiliaryFloorColor | Returns or sets the auxiliary floor |
AuxiliaryFloorColorSelection | Returns or sets the auxiliary floor selection. |
BladeBlendColor | Returns or sets the blade blend color |
BladeColor | Returns or sets the blade color |
BlankColor | Returns or sets the blank color |
BlankSelection | Returns or sets the blank selection. |
CheckColor | Returns or sets the check color |
CheckSelection | Returns or sets the check selection. |
ClearanceColor | Returns or sets the clearance color |
ClsfDecimals | Returns or sets the clsf_decimals |
ClsfForceLoadTurret | Returns or sets the force load turret |
ConfigurationFile | Returns or sets the configuration file |
CsysInformationListing | Returns or sets the base info |
CsysOrientWcsToMcs | Returns or sets the orient wcs to mcs |
CutAreaColor | Returns or sets the cut area color |
CutAreaSelection | Returns or sets the cut area selection. |
DisplaySelectedObjects | Returns or sets the display selected objects |
DisplayTurningIpw | Returns or sets the display turning ipw |
DriveColor | Returns or sets the drive color |
EnableLevelBasedIpw | Returns or sets the enable level based ipw |
ForceRegenerate | Returns or sets the force regenerate |
GeneratePaths | Returns or sets the generate tool paths |
GenerationFullRegeneration | Returns or sets the full regeneration |
GenerationPauseAfterEachPath | Returns or sets the pause after each path |
GenerationRefreshBeforeEachPath | Returns or sets the refresh before each path |
GenerationSmartRegeneration | Returns or sets the smart regeneration |
GenerationUpdateInstances | Returns or sets the update all instances |
HubColor | Returns or sets the hub color |
IncludeInstances | Returns or sets the include instances |
IpwNeedleCountCoarse | Returns or sets the coarse ipw needle count |
IpwNeedleCountFine | Returns or sets the fine ipw needle count |
IpwNeedleCountMedium | Returns or sets the medium ipw needle count |
IpwNeedleDistanceCoarse | Returns or sets the coarse ipw needle distance |
IpwNeedleDistanceFine | Returns or sets the fine ipw needle distance |
IpwNeedleDistanceMedium | Returns or sets the medium ipw needle distance |
IpwPartsFolder | Returns or sets the ipw parts folder |
IpwToleranceMode | Returns or sets the ipw tolerance mode |
IpwUseDirectoryOfOriginalPart | Returns or sets the use directory original part |
LinkMcsRcs | Returns or sets the link mcs rcs |
OptimizedCutLevelColor | Returns or sets the optimized cut level |
PartColor | Returns or sets the part color |
PartSelection | Returns or sets the part selection. |
RelocateParameters | Returns or sets the relocate parameters |
ReplayRefreshBeforeEachPath | Returns or sets the refresh before each path replay |
RunProcessAssistant | Returns or sets the process assistant |
SaveIpwModel | Returns or sets the ipw model |
SaveLevelBasedIpw | Returns or sets the level based ipw |
ScrollAreaSize | Returns or sets the scrollable items |
ShowPictures | Returns or sets the show pictures |
ShroudColor | Returns or sets the shroud color |
SplitterColor | Returns or sets the splitter color |
StepoverDisplayAsNCM | Returns or sets the stepover move display as non cutting move |
SuspectBoundingBoxColor | Returns or sets the suspect bounding box color |
Tag | Returns the Tag for this object. |
TemplateFile | Returns or sets the template file |
TopOffLevelColor | Returns or sets the top off level |
TrimColor | Returns or sets the trim color |
UncutRegionColor | Returns or sets the uncut region color |
UnlinkInstances | Returns or sets the unlink instances |
Visualize2dTool1Color | Returns or sets the tool color1 |
Visualize2dTool2Color | Returns or sets the tool color2 |
Visualize2dTool3Color | Returns or sets the tool color3 |
Visualize2dTool4Color | Returns or sets the tool color4 |
Visualize2dTool5Color | Returns or sets the tool color5 |
VisualizeAnimationAccuracy | Returns or sets the animation accuracy |
VisualizeAutoBlockColor | Returns or sets the auto block color |
VisualizeBackgroundColor | Returns or sets the background color |
VisualizeChordalTolerance | Returns or sets the chordal tolerance |
VisualizeCollisionsColor | Returns or sets the collisions color |
VisualizeDynamicToolAxis | Returns or sets the dynamic tool axis |
VisualizeExcessMaterialColor | Returns or sets the excess material color |
VisualizeGougesColor | Returns or sets the gouges color |
VisualizeIpwColor | Returns or sets the ipw color |
VisualizeIpwDmrColor1 | Returns or sets the ipw dmr color1 |
VisualizeIpwDmrColor10 | Returns or sets the ipw dmr color10 |
VisualizeIpwDmrColor2 | Returns or sets the ipw dmr color2 |
VisualizeIpwDmrColor3 | Returns or sets the ipw dmr color3 |
VisualizeIpwDmrColor4 | Returns or sets the ipw dmr color4 |
VisualizeIpwDmrColor5 | Returns or sets the ipw dmr color5 |
VisualizeIpwDmrColor6 | Returns or sets the ipw dmr color6 |
VisualizeIpwDmrColor7 | Returns or sets the ipw dmr color7 |
VisualizeIpwDmrColor8 | Returns or sets the ipw dmr color8 |
VisualizeIpwDmrColor9 | Returns or sets the ipw dmr color9 |
VisualizeIpwDmrColoringMode | Returns or sets the ipw dmr coloring mode |
VisualizeIpwTranslucency | Returns or sets the ipw translucency |
VisualizeSafeToolColor | Returns or sets the safe tool color |
VisualizeTemporaryContainmentCurveColor | Returns or sets the temporary containment curve color |
VisualizeToolAxisTiltTolerance | Returns or sets the tilt tolerance |
VisualizeToolDisplayColor | Returns or sets the tool display color |
VisualizeToolEditAndDisplay | Returns or sets the tool edit and display |
VisualizeToolHolderColor | Returns or sets the tool holder color |
VisualizeToolInsertOrFluteColor | Returns or sets the turning tool insert |
VisualizeToolShankColor | Returns or sets the tool shank color |
VisualizeToolTranslucency | Returns or sets the tool translucency |
WallColor | Returns or sets the wall color |
WallSelection | Returns or sets the wall selection. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDefaultConfigurationFile | Get the default configuration file |
GetDefaultIpwFolder | Get the ipw default folder |
GetDefaultTemplateFile | Get the default template file |
GetObject | Returns the object currently being edited by this builder. |
GetSelection | The geometry selection type method |
SetSelection | The geometry selection type method |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreferencesAnimationAccuracyTypes Enumeration | the animation accuracy types |
PreferencesAuxiliaryFloorColorSelectionTypes Enumeration | the auxiliary floor selection types. |
PreferencesBlankSelectionTypes Enumeration | the blank selection types. |
PreferencesCheckSelectionTypes Enumeration | the check selection types. |
PreferencesCsysInformationListingTypes Enumeration | the information listing types |
PreferencesCutAreaSelectionTypes Enumeration | the cut area selection types. |
PreferencesGeometryTypes Enumeration | the geometry types |
PreferencesIpwDmrColoringTypes Enumeration | the IPW material removal coloring types |
PreferencesIpwToleranceModeTypes Enumeration | the IPW tolerance modes |
PreferencesPartSelectionTypes Enumeration | the part selection types. |
PreferencesSelectionTypes Enumeration | the selection types |
PreferencesWallSelectionTypes Enumeration | the wall selection types. |
Property Detail¶
AlwaysUpdateDialogs¶
-
Preferences.
AlwaysUpdateDialogs
¶ Returns or sets the auto update dialog
-------------------------------------
Getter Method
Signature
AlwaysUpdateDialogs
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlwaysUpdateDialogs
Parameters: alwaysUpdateDialogs (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AutomaticallySetMachingData¶
-
Preferences.
AutomaticallySetMachingData
¶ Returns or sets the auto maching data
-------------------------------------
Getter Method
Signature
AutomaticallySetMachingData
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutomaticallySetMachingData
Parameters: autoMachingData (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AuxiliaryFloorColor¶
-
Preferences.
AuxiliaryFloorColor
¶ Returns or sets the auxiliary floor
-------------------------------------
Getter Method
Signature
AuxiliaryFloorColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AuxiliaryFloorColor
Parameters: auxiliaryFloor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
AuxiliaryFloorColorSelection¶
-
Preferences.
AuxiliaryFloorColorSelection
¶ Returns or sets the auxiliary floor selection.
-------------------------------------
Getter Method
Signature
AuxiliaryFloorColorSelection
Returns: Return type: NXOpen.CAM.PreferencesAuxiliaryFloorColorSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
AuxiliaryFloorColorSelection
Parameters: auxiliaryFloorSelection ( NXOpen.CAM.PreferencesAuxiliaryFloorColorSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
BladeBlendColor¶
-
Preferences.
BladeBlendColor
¶ Returns or sets the blade blend color
-------------------------------------
Getter Method
Signature
BladeBlendColor
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BladeBlendColor
Parameters: bladeBlend (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
BladeColor¶
-
Preferences.
BladeColor
¶ Returns or sets the blade color
-------------------------------------
Getter Method
Signature
BladeColor
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BladeColor
Parameters: blade (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
BlankColor¶
-
Preferences.
BlankColor
¶ Returns or sets the blank color
-------------------------------------
Getter Method
Signature
BlankColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankColor
Parameters: blankColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
BlankSelection¶
-
Preferences.
BlankSelection
¶ Returns or sets the blank selection.
-------------------------------------
Getter Method
Signature
BlankSelection
Returns: Return type: NXOpen.CAM.PreferencesBlankSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
BlankSelection
Parameters: blankSelection ( NXOpen.CAM.PreferencesBlankSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
CheckColor¶
-
Preferences.
CheckColor
¶ Returns or sets the check color
-------------------------------------
Getter Method
Signature
CheckColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckColor
Parameters: checkColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CheckSelection¶
-
Preferences.
CheckSelection
¶ Returns or sets the check selection.
-------------------------------------
Getter Method
Signature
CheckSelection
Returns: Return type: NXOpen.CAM.PreferencesCheckSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
CheckSelection
Parameters: checkSelection ( NXOpen.CAM.PreferencesCheckSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
ClearanceColor¶
-
Preferences.
ClearanceColor
¶ Returns or sets the clearance color
-------------------------------------
Getter Method
Signature
ClearanceColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceColor
Parameters: clearanceColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ClsfDecimals¶
-
Preferences.
ClsfDecimals
¶ Returns or sets the clsf_decimals
-------------------------------------
Getter Method
Signature
ClsfDecimals
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClsfDecimals
Parameters: decimals (int) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ClsfForceLoadTurret¶
-
Preferences.
ClsfForceLoadTurret
¶ Returns or sets the force load turret
-------------------------------------
Getter Method
Signature
ClsfForceLoadTurret
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClsfForceLoadTurret
Parameters: forceLoadTurret (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ConfigurationFile¶
-
Preferences.
ConfigurationFile
¶ Returns or sets the configuration file
-------------------------------------
Getter Method
Signature
ConfigurationFile
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConfigurationFile
Parameters: fileName (str) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CsysInformationListing¶
-
Preferences.
CsysInformationListing
¶ Returns or sets the base info
-------------------------------------
Getter Method
Signature
CsysInformationListing
Returns: Return type: NXOpen.CAM.PreferencesCsysInformationListingTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysInformationListing
Parameters: baseInfo ( NXOpen.CAM.PreferencesCsysInformationListingTypes
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CsysOrientWcsToMcs¶
-
Preferences.
CsysOrientWcsToMcs
¶ Returns or sets the orient wcs to mcs
-------------------------------------
Getter Method
Signature
CsysOrientWcsToMcs
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysOrientWcsToMcs
Parameters: orientWcsToMcs (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutAreaColor¶
-
Preferences.
CutAreaColor
¶ Returns or sets the cut area color
-------------------------------------
Getter Method
Signature
CutAreaColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutAreaColor
Parameters: cutAreaColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
CutAreaSelection¶
-
Preferences.
CutAreaSelection
¶ Returns or sets the cut area selection.
-------------------------------------
Getter Method
Signature
CutAreaSelection
Returns: Return type: NXOpen.CAM.PreferencesCutAreaSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
CutAreaSelection
Parameters: cutAreaSelection ( NXOpen.CAM.PreferencesCutAreaSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
DisplaySelectedObjects¶
-
Preferences.
DisplaySelectedObjects
¶ Returns or sets the display selected objects
-------------------------------------
Getter Method
Signature
DisplaySelectedObjects
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplaySelectedObjects
Parameters: displaySelectedObjects (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
DisplayTurningIpw¶
-
Preferences.
DisplayTurningIpw
¶ Returns or sets the display turning ipw
-------------------------------------
Getter Method
Signature
DisplayTurningIpw
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayTurningIpw
Parameters: displayTurningIpw (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
DriveColor¶
-
Preferences.
DriveColor
¶ Returns or sets the drive color
-------------------------------------
Getter Method
Signature
DriveColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DriveColor
Parameters: driveColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
EnableLevelBasedIpw¶
-
Preferences.
EnableLevelBasedIpw
¶ Returns or sets the enable level based ipw
-------------------------------------
Getter Method
Signature
EnableLevelBasedIpw
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EnableLevelBasedIpw
Parameters: enableLevelBasedIpw (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ForceRegenerate¶
-
Preferences.
ForceRegenerate
¶ Returns or sets the force regenerate
-------------------------------------
Getter Method
Signature
ForceRegenerate
Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForceRegenerate
Parameters: isForceRegenerate (bool) – New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
GeneratePaths¶
-
Preferences.
GeneratePaths
¶ Returns or sets the generate tool paths
-------------------------------------
Getter Method
Signature
GeneratePaths
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeneratePaths
Parameters: generatePaths (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GenerationFullRegeneration¶
-
Preferences.
GenerationFullRegeneration
¶ Returns or sets the full regeneration
-------------------------------------
Getter Method
Signature
GenerationFullRegeneration
Returns: Return type: bool New in version NX9.0.3.
Deprecated since version NX10.0.3: Use
CAM.Preferences.GenerationSmartRegeneration()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationFullRegeneration
Parameters: fullRegeneration (bool) – New in version NX9.0.3.
Deprecated since version NX10.0.3: Use
CAM.Preferences.GenerationSmartRegeneration()
instead.License requirements: cam_base (“CAM BASE”)
GenerationPauseAfterEachPath¶
-
Preferences.
GenerationPauseAfterEachPath
¶ Returns or sets the pause after each path
-------------------------------------
Getter Method
Signature
GenerationPauseAfterEachPath
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationPauseAfterEachPath
Parameters: pauseAfterEachPath (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GenerationRefreshBeforeEachPath¶
-
Preferences.
GenerationRefreshBeforeEachPath
¶ Returns or sets the refresh before each path
-------------------------------------
Getter Method
Signature
GenerationRefreshBeforeEachPath
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationRefreshBeforeEachPath
Parameters: refreshBeforeEachPath (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GenerationSmartRegeneration¶
-
Preferences.
GenerationSmartRegeneration
¶ Returns or sets the smart regeneration
-------------------------------------
Getter Method
Signature
GenerationSmartRegeneration
Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationSmartRegeneration
Parameters: smartRegeneration (bool) – New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
GenerationUpdateInstances¶
-
Preferences.
GenerationUpdateInstances
¶ Returns or sets the update all instances
-------------------------------------
Getter Method
Signature
GenerationUpdateInstances
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GenerationUpdateInstances
Parameters: updateInstances (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
HubColor¶
-
Preferences.
HubColor
¶ Returns or sets the hub color
-------------------------------------
Getter Method
Signature
HubColor
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HubColor
Parameters: hub (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
IncludeInstances¶
-
Preferences.
IncludeInstances
¶ Returns or sets the include instances
-------------------------------------
Getter Method
Signature
IncludeInstances
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeInstances
Parameters: includeInstances (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
IpwNeedleCountCoarse¶
-
Preferences.
IpwNeedleCountCoarse
¶ Returns or sets the coarse ipw needle count
-------------------------------------
Getter Method
Signature
IpwNeedleCountCoarse
Returns: Return type: int New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleCountCoarse
Parameters: count (int) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleCountFine¶
-
Preferences.
IpwNeedleCountFine
¶ Returns or sets the fine ipw needle count
-------------------------------------
Getter Method
Signature
IpwNeedleCountFine
Returns: Return type: int New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleCountFine
Parameters: count (int) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleCountMedium¶
-
Preferences.
IpwNeedleCountMedium
¶ Returns or sets the medium ipw needle count
-------------------------------------
Getter Method
Signature
IpwNeedleCountMedium
Returns: Return type: int New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleCountMedium
Parameters: count (int) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleDistanceCoarse¶
-
Preferences.
IpwNeedleDistanceCoarse
¶ Returns or sets the coarse ipw needle distance
-------------------------------------
Getter Method
Signature
IpwNeedleDistanceCoarse
Returns: Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleDistanceCoarse
Parameters: distance (float) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleDistanceFine¶
-
Preferences.
IpwNeedleDistanceFine
¶ Returns or sets the fine ipw needle distance
-------------------------------------
Getter Method
Signature
IpwNeedleDistanceFine
Returns: Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleDistanceFine
Parameters: distance (float) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwNeedleDistanceMedium¶
-
Preferences.
IpwNeedleDistanceMedium
¶ Returns or sets the medium ipw needle distance
-------------------------------------
Getter Method
Signature
IpwNeedleDistanceMedium
Returns: Return type: float New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwNeedleDistanceMedium
Parameters: distance (float) – New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwPartsFolder¶
-
Preferences.
IpwPartsFolder
¶ Returns or sets the ipw parts folder
-------------------------------------
Getter Method
Signature
IpwPartsFolder
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwPartsFolder
Parameters: foldername (str) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
IpwToleranceMode¶
-
Preferences.
IpwToleranceMode
¶ Returns or sets the ipw tolerance mode
-------------------------------------
Getter Method
Signature
IpwToleranceMode
Returns: Return type: NXOpen.CAM.PreferencesIpwToleranceModeTypes
New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwToleranceMode
Parameters: mode ( NXOpen.CAM.PreferencesIpwToleranceModeTypes
) –New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
IpwUseDirectoryOfOriginalPart¶
-
Preferences.
IpwUseDirectoryOfOriginalPart
¶ Returns or sets the use directory original part
-------------------------------------
Getter Method
Signature
IpwUseDirectoryOfOriginalPart
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IpwUseDirectoryOfOriginalPart
Parameters: useIpwDirectoryOfOriginalPart (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
LinkMcsRcs¶
-
Preferences.
LinkMcsRcs
¶ Returns or sets the link mcs rcs
-------------------------------------
Getter Method
Signature
LinkMcsRcs
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinkMcsRcs
Parameters: linkMcsRcs (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
OptimizedCutLevelColor¶
-
Preferences.
OptimizedCutLevelColor
¶ Returns or sets the optimized cut level
-------------------------------------
Getter Method
Signature
OptimizedCutLevelColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OptimizedCutLevelColor
Parameters: optimizedCutLevel (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
PartColor¶
-
Preferences.
PartColor
¶ Returns or sets the part color
-------------------------------------
Getter Method
Signature
PartColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartColor
Parameters: partColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
PartSelection¶
-
Preferences.
PartSelection
¶ Returns or sets the part selection.
-------------------------------------
Getter Method
Signature
PartSelection
Returns: Return type: NXOpen.CAM.PreferencesPartSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
PartSelection
Parameters: partSelection ( NXOpen.CAM.PreferencesPartSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
RelocateParameters¶
-
Preferences.
RelocateParameters
¶ Returns or sets the relocate parameters
-------------------------------------
Getter Method
Signature
RelocateParameters
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RelocateParameters
Parameters: relocateParameters (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ReplayRefreshBeforeEachPath¶
-
Preferences.
ReplayRefreshBeforeEachPath
¶ Returns or sets the refresh before each path replay
-------------------------------------
Getter Method
Signature
ReplayRefreshBeforeEachPath
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReplayRefreshBeforeEachPath
Parameters: refreshBeforeEachPath (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
RunProcessAssistant¶
-
Preferences.
RunProcessAssistant
¶ Returns or sets the process assistant
-------------------------------------
Getter Method
Signature
RunProcessAssistant
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RunProcessAssistant
Parameters: processAssistant (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SaveIpwModel¶
-
Preferences.
SaveIpwModel
¶ Returns or sets the ipw model
-------------------------------------
Getter Method
Signature
SaveIpwModel
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveIpwModel
Parameters: ipwModel (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
SaveLevelBasedIpw¶
-
Preferences.
SaveLevelBasedIpw
¶ Returns or sets the level based ipw
-------------------------------------
Getter Method
Signature
SaveLevelBasedIpw
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveLevelBasedIpw
Parameters: levelBasedIpw (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ScrollAreaSize¶
-
Preferences.
ScrollAreaSize
¶ Returns or sets the scrollable items
-------------------------------------
Getter Method
Signature
ScrollAreaSize
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ScrollAreaSize
Parameters: scrollableItems (int) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ShowPictures¶
-
Preferences.
ShowPictures
¶ Returns or sets the show pictures
-------------------------------------
Getter Method
Signature
ShowPictures
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowPictures
Parameters: showPictures (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ShroudColor¶
-
Preferences.
ShroudColor
¶ Returns or sets the shroud color
-------------------------------------
Getter Method
Signature
ShroudColor
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShroudColor
Parameters: shroud (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
SplitterColor¶
-
Preferences.
SplitterColor
¶ Returns or sets the splitter color
-------------------------------------
Getter Method
Signature
SplitterColor
Returns: Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SplitterColor
Parameters: splitter (Id) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
StepoverDisplayAsNCM¶
-
Preferences.
StepoverDisplayAsNCM
¶ Returns or sets the stepover move display as non cutting move
-------------------------------------
Getter Method
Signature
StepoverDisplayAsNCM
Returns: Return type: bool New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepoverDisplayAsNCM
Parameters: bStepOverAsNCM (bool) – New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
SuspectBoundingBoxColor¶
-
Preferences.
SuspectBoundingBoxColor
¶ Returns or sets the suspect bounding box color
-------------------------------------
Getter Method
Signature
SuspectBoundingBoxColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SuspectBoundingBoxColor
Parameters: suspectBoundingBoxColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TemplateFile¶
-
Preferences.
TemplateFile
¶ Returns or sets the template file
-------------------------------------
Getter Method
Signature
TemplateFile
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemplateFile
Parameters: fileName (str) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TopOffLevelColor¶
-
Preferences.
TopOffLevelColor
¶ Returns or sets the top off level
-------------------------------------
Getter Method
Signature
TopOffLevelColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TopOffLevelColor
Parameters: topOffLevel (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TrimColor¶
-
Preferences.
TrimColor
¶ Returns or sets the trim color
-------------------------------------
Getter Method
Signature
TrimColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimColor
Parameters: trimColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
UncutRegionColor¶
-
Preferences.
UncutRegionColor
¶ Returns or sets the uncut region color
-------------------------------------
Getter Method
Signature
UncutRegionColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UncutRegionColor
Parameters: uncutRegionColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
UnlinkInstances¶
-
Preferences.
UnlinkInstances
¶ Returns or sets the unlink instances
-------------------------------------
Getter Method
Signature
UnlinkInstances
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UnlinkInstances
Parameters: unlinkInstances (bool) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Visualize2dTool1Color¶
-
Preferences.
Visualize2dTool1Color
¶ Returns or sets the tool color1
-------------------------------------
Getter Method
Signature
Visualize2dTool1Color
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor1()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool1Color
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor1()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool2Color¶
-
Preferences.
Visualize2dTool2Color
¶ Returns or sets the tool color2
-------------------------------------
Getter Method
Signature
Visualize2dTool2Color
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor2()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool2Color
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor2()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool3Color¶
-
Preferences.
Visualize2dTool3Color
¶ Returns or sets the tool color3
-------------------------------------
Getter Method
Signature
Visualize2dTool3Color
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor3()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool3Color
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor3()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool4Color¶
-
Preferences.
Visualize2dTool4Color
¶ Returns or sets the tool color4
-------------------------------------
Getter Method
Signature
Visualize2dTool4Color
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor4()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool4Color
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor4()
instead.License requirements: cam_base (“CAM BASE”)
Visualize2dTool5Color¶
-
Preferences.
Visualize2dTool5Color
¶ Returns or sets the tool color5
-------------------------------------
Getter Method
Signature
Visualize2dTool5Color
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor5()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Visualize2dTool5Color
Parameters: toolColor (Id) – New in version NX7.5.0.
Deprecated since version NX9.0.0: Use
CAM.Preferences.VisualizeIpwDmrColor5()
instead.License requirements: cam_base (“CAM BASE”)
VisualizeAnimationAccuracy¶
-
Preferences.
VisualizeAnimationAccuracy
¶ Returns or sets the animation accuracy
-------------------------------------
Getter Method
Signature
VisualizeAnimationAccuracy
Returns: Return type: NXOpen.CAM.PreferencesAnimationAccuracyTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeAnimationAccuracy
Parameters: animationAccuracy ( NXOpen.CAM.PreferencesAnimationAccuracyTypes
) –New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeAutoBlockColor¶
-
Preferences.
VisualizeAutoBlockColor
¶ Returns or sets the auto block color
-------------------------------------
Getter Method
Signature
VisualizeAutoBlockColor
Returns: Return type: Id New in version NX7.5.0.
Deprecated since version NX8.5.0: Use
CAM.Preferences.BlankColor()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeAutoBlockColor
Parameters: autoBlockColor (Id) – New in version NX7.5.0.
Deprecated since version NX8.5.0: Use
CAM.Preferences.BlankColor()
instead.License requirements: cam_base (“CAM BASE”)
VisualizeBackgroundColor¶
-
Preferences.
VisualizeBackgroundColor
¶ Returns or sets the background color
-------------------------------------
Getter Method
Signature
VisualizeBackgroundColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeBackgroundColor
Parameters: backgroundColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeChordalTolerance¶
-
Preferences.
VisualizeChordalTolerance
¶ Returns or sets the chordal tolerance
-------------------------------------
Getter Method
Signature
VisualizeChordalTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeChordalTolerance
Parameters: chordalTolerance (float) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeCollisionsColor¶
-
Preferences.
VisualizeCollisionsColor
¶ Returns or sets the collisions color
-------------------------------------
Getter Method
Signature
VisualizeCollisionsColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeCollisionsColor
Parameters: collisionsColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeDynamicToolAxis¶
-
Preferences.
VisualizeDynamicToolAxis
¶ Returns or sets the dynamic tool axis
-------------------------------------
Getter Method
Signature
VisualizeDynamicToolAxis
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeDynamicToolAxis
Parameters: dynToolAxis (bool) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeExcessMaterialColor¶
-
Preferences.
VisualizeExcessMaterialColor
¶ Returns or sets the excess material color
-------------------------------------
Getter Method
Signature
VisualizeExcessMaterialColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeExcessMaterialColor
Parameters: excessMaterialColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeGougesColor¶
-
Preferences.
VisualizeGougesColor
¶ Returns or sets the gouges color
-------------------------------------
Getter Method
Signature
VisualizeGougesColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeGougesColor
Parameters: gougesColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwColor¶
-
Preferences.
VisualizeIpwColor
¶ Returns or sets the ipw color
-------------------------------------
Getter Method
Signature
VisualizeIpwColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwColor
Parameters: ipwColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor1¶
-
Preferences.
VisualizeIpwDmrColor1
¶ Returns or sets the ipw dmr color1
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor1
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor1
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor10¶
-
Preferences.
VisualizeIpwDmrColor10
¶ Returns or sets the ipw dmr color10
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor10
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor10
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor2¶
-
Preferences.
VisualizeIpwDmrColor2
¶ Returns or sets the ipw dmr color2
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor2
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor2
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor3¶
-
Preferences.
VisualizeIpwDmrColor3
¶ Returns or sets the ipw dmr color3
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor3
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor3
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor4¶
-
Preferences.
VisualizeIpwDmrColor4
¶ Returns or sets the ipw dmr color4
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor4
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor4
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor5¶
-
Preferences.
VisualizeIpwDmrColor5
¶ Returns or sets the ipw dmr color5
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor5
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor5
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor6¶
-
Preferences.
VisualizeIpwDmrColor6
¶ Returns or sets the ipw dmr color6
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor6
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor6
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor7¶
-
Preferences.
VisualizeIpwDmrColor7
¶ Returns or sets the ipw dmr color7
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor7
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor7
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor8¶
-
Preferences.
VisualizeIpwDmrColor8
¶ Returns or sets the ipw dmr color8
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor8
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor8
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColor9¶
-
Preferences.
VisualizeIpwDmrColor9
¶ Returns or sets the ipw dmr color9
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColor9
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColor9
Parameters: ipwColor (Id) – New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwDmrColoringMode¶
-
Preferences.
VisualizeIpwDmrColoringMode
¶ Returns or sets the ipw dmr coloring mode
-------------------------------------
Getter Method
Signature
VisualizeIpwDmrColoringMode
Returns: Return type: NXOpen.CAM.PreferencesIpwDmrColoringTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwDmrColoringMode
Parameters: coloring ( NXOpen.CAM.PreferencesIpwDmrColoringTypes
) –New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeIpwTranslucency¶
-
Preferences.
VisualizeIpwTranslucency
¶ Returns or sets the ipw translucency
-------------------------------------
Getter Method
Signature
VisualizeIpwTranslucency
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeIpwTranslucency
Parameters: ipwTranslucency (int) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeSafeToolColor¶
-
Preferences.
VisualizeSafeToolColor
¶ Returns or sets the safe tool color
-------------------------------------
Getter Method
Signature
VisualizeSafeToolColor
Returns: Return type: Id New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeSafeToolColor
Parameters: safeToolColor (Id) – New in version NX7.5.2.
License requirements: cam_base (“CAM BASE”)
VisualizeTemporaryContainmentCurveColor¶
-
Preferences.
VisualizeTemporaryContainmentCurveColor
¶ Returns or sets the temporary containment curve color
-------------------------------------
Getter Method
Signature
VisualizeTemporaryContainmentCurveColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeTemporaryContainmentCurveColor
Parameters: temporaryContainmentCurveColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolAxisTiltTolerance¶
-
Preferences.
VisualizeToolAxisTiltTolerance
¶ Returns or sets the tilt tolerance
-------------------------------------
Getter Method
Signature
VisualizeToolAxisTiltTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolAxisTiltTolerance
Parameters: tiltTolerance (float) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolDisplayColor¶
-
Preferences.
VisualizeToolDisplayColor
¶ Returns or sets the tool display color
-------------------------------------
Getter Method
Signature
VisualizeToolDisplayColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolDisplayColor
Parameters: toolDisplayColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolEditAndDisplay¶
-
Preferences.
VisualizeToolEditAndDisplay
¶ Returns or sets the tool edit and display
-------------------------------------
Getter Method
Signature
VisualizeToolEditAndDisplay
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolEditAndDisplay
Parameters: toolDisplayColor (bool) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolHolderColor¶
-
Preferences.
VisualizeToolHolderColor
¶ Returns or sets the tool holder color
-------------------------------------
Getter Method
Signature
VisualizeToolHolderColor
Returns: holder color Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolHolderColor
Parameters: holderColor (Id) – holder color New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolInsertOrFluteColor¶
-
Preferences.
VisualizeToolInsertOrFluteColor
¶ Returns or sets the turning tool insert
-------------------------------------
Getter Method
Signature
VisualizeToolInsertOrFluteColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolInsertOrFluteColor
Parameters: color (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolShankColor¶
-
Preferences.
VisualizeToolShankColor
¶ Returns or sets the tool shank color
-------------------------------------
Getter Method
Signature
VisualizeToolShankColor
Returns: shank color Return type: Id New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolShankColor
Parameters: shankColor (Id) – shank color New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
VisualizeToolTranslucency¶
-
Preferences.
VisualizeToolTranslucency
¶ Returns or sets the tool translucency
-------------------------------------
Getter Method
Signature
VisualizeToolTranslucency
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisualizeToolTranslucency
Parameters: toolTranslucency (int) – New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
WallColor¶
-
Preferences.
WallColor
¶ Returns or sets the wall color
-------------------------------------
Getter Method
Signature
WallColor
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WallColor
Parameters: wallColor (Id) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
WallSelection¶
-
Preferences.
WallSelection
¶ Returns or sets the wall selection.
-------------------------------------
Getter Method
Signature
WallSelection
Returns: Return type: NXOpen.CAM.PreferencesWallSelectionTypes
New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
WallSelection
Parameters: wallSelection ( NXOpen.CAM.PreferencesWallSelectionTypes
) –New in version NX7.5.0.
Deprecated since version NX8.0.0: Use
CAM.Preferences.GetSelection()
andCAM.Preferences.SetSelection()
instead.License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetDefaultConfigurationFile¶
-
Preferences.
GetDefaultConfigurationFile
¶ Get the default configuration file
Signature
GetDefaultConfigurationFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
GetDefaultIpwFolder¶
-
Preferences.
GetDefaultIpwFolder
¶ Get the ipw default folder
Signature
GetDefaultIpwFolder()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
GetDefaultTemplateFile¶
-
Preferences.
GetDefaultTemplateFile
¶ Get the default template file
Signature
GetDefaultTemplateFile()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
GetSelection¶
-
Preferences.
GetSelection
¶ The geometry selection type method
Signature
GetSelection(geomType)
Parameters: geomType ( NXOpen.CAM.PreferencesGeometryTypes
) –Returns: Return type: NXOpen.CAM.PreferencesSelectionTypes
New in version NX8.0.0.
License requirements: None.
SetSelection¶
-
Preferences.
SetSelection
¶ The geometry selection type method
Signature
SetSelection(geomType, selection)
Parameters: - geomType (
NXOpen.CAM.PreferencesGeometryTypes
) – - selection (
NXOpen.CAM.PreferencesSelectionTypes
) –
New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
- geomType (
Validate¶
-
Preferences.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.