CAMSession Class¶
-
class
NXOpen.CAM.
CAMSession
¶ Bases:
object
Represents cam session
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX4.0.0.
“PathDisplay”, “Returns the
NXOpen.CAM.PathDisplay
belonging to this cam session “
Methods¶
Method | Description |
---|---|
CreateCamPreferences | Create Cam Preferences builder. |
GetMcsDisplay | Get MCS display |
GetTemplateSubtypes | Get the names of the available template subypes for the specified template type. |
GetTemplateTypes | Get the names of the available template types. |
SetMcsDisplay | Set MCS display |
SpecifyConfiguration | Specify the configuration file of the current cam session |
Enumerations¶
CAMSessionObjectSubtype Enumeration | the template subtype class |
PathDisplay¶
-
CAMSession.
PathDisplay
¶ Returns the
NXOpen.CAM.PathDisplay
belonging to this cam sessionSignature
PathDisplay
New in version NX10.0.2.
Returns: Return type: NXOpen.CAM.PathDisplay
Method Detail¶
CreateCamPreferences¶
-
CAMSession.
CreateCamPreferences
¶ Create Cam Preferences builder.
Signature
CreateCamPreferences()
Returns: created cam preferences builder Return type: NXOpen.CAM.Preferences
New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
GetMcsDisplay¶
-
CAMSession.
GetMcsDisplay
¶ Get MCS display
Signature
GetMcsDisplay()
Returns: whether the MCS should be displayed Return type: bool New in version NX8.0.1.
License requirements: None.
GetTemplateSubtypes¶
-
CAMSession.
GetTemplateSubtypes
¶ Get the names of the available template subypes for the specified template type.
Only those subtypes have the specified subtype class are returned.
Signature
GetTemplateSubtypes(typeName, subtypeClass)
Parameters: - typeName (str) – the name of the template type
- subtypeClass (
NXOpen.CAM.CAMSessionObjectSubtype
) – the subtype class
Returns: the names of available subtypes
Return type: list of str
New in version NX4.0.0.
License requirements: cam_base (“CAM BASE”)
GetTemplateTypes¶
-
CAMSession.
GetTemplateTypes
¶ Get the names of the available template types.
Signature
GetTemplateTypes()
Returns: the names of the template types Return type: list of str New in version NX4.0.0.
License requirements: cam_base (“CAM BASE”)