PathDisplay Class¶
-
class
NXOpen.CAM.
PathDisplay
¶ Bases:
object
Represents a class that is used for NX testing.
This class should not be made available to customers To obtain an instance of this class, refer to
NXOpen.CAM.CAMSession
New in version NX10.0.2.
Properties¶
Property | Description |
---|---|
ColorBy | Returns or sets the color by property |
ShowCutting | Returns or sets the indicator to display only cutting moves in a tool path. |
ShowEndpoints | Returns or sets the indicator to display symbol at the end of each motion. |
ShowNoncutting | Returns or sets the indicator to display only non cutting moves in a tool path. |
ShowToolCenter | Returns or sets the indicator to display tool path at the tool center instead of the tool tip for a ball mill. |
Methods¶
Method | Description |
---|---|
HideToolPath | Hide tool path |
ShowToolPath | Show tool path |
Enumerations¶
PathDisplayColorByType Enumeration | Choices for coloring the tool path motions |
Property Detail¶
ColorBy¶
-
PathDisplay.
ColorBy
¶ Returns or sets the color by property
-------------------------------------
Getter Method
Signature
ColorBy
Returns: Return type: NXOpen.CAM.PathDisplayColorByType
New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColorBy
Parameters: colorBy ( NXOpen.CAM.PathDisplayColorByType
) –New in version NX10.0.2.
License requirements: None.
ShowCutting¶
-
PathDisplay.
ShowCutting
¶ Returns or sets the indicator to display only cutting moves in a tool path.
-------------------------------------
Getter Method
Signature
ShowCutting
Returns: Return type: bool New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowCutting
Parameters: isOn (bool) – New in version NX10.0.2.
License requirements: None.
ShowEndpoints¶
-
PathDisplay.
ShowEndpoints
¶ Returns or sets the indicator to display symbol at the end of each motion.
-------------------------------------
Getter Method
Signature
ShowEndpoints
Returns: Return type: bool New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowEndpoints
Parameters: isOn (bool) – New in version NX10.0.2.
License requirements: None.
ShowNoncutting¶
-
PathDisplay.
ShowNoncutting
¶ Returns or sets the indicator to display only non cutting moves in a tool path.
-------------------------------------
Getter Method
Signature
ShowNoncutting
Returns: Return type: bool New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowNoncutting
Parameters: isOn (bool) – New in version NX10.0.2.
License requirements: None.
ShowToolCenter¶
-
PathDisplay.
ShowToolCenter
¶ Returns or sets the indicator to display tool path at the tool center instead of the tool tip for a ball mill.
-------------------------------------
Getter Method
Signature
ShowToolCenter
Returns: Return type: bool New in version NX10.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowToolCenter
Parameters: isOn (bool) – New in version NX10.0.2.
License requirements: None.
Method Detail¶
HideToolPath¶
-
PathDisplay.
HideToolPath
¶ Hide tool path
Signature
HideToolPath(opr)
Parameters: opr ( NXOpen.CAM.CAMObject
) –New in version NX10.0.2.
License requirements: None.
ShowToolPath¶
-
PathDisplay.
ShowToolPath
¶ Show tool path
Signature
ShowToolPath(opr)
Parameters: opr ( NXOpen.CAM.CAMObject
) –New in version NX10.0.2.
License requirements: None.