PathDisplayColorByType Enumeration

NXOpen.CAM.PathDisplay.ColorByType is an alias for NXOpen.CAM.PathDisplayColorByType

class NXOpen.CAM.PathDisplayColorByType

Bases: object

Choices for coloring the tool path motions

Enum Members

Enum Member Enum Member Description
MotionType
Operation
Tool
MotionLength
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.