PreferencesSelectionTypes Enumeration¶
NXOpen.CAM.Preferences.SelectionTypes is an alias for NXOpen.CAM.PreferencesSelectionTypes
-
class
NXOpen.CAM.
PreferencesSelectionTypes
¶ Bases:
object
the selection types
Enum Members
Enum Member Enum Member Description NoSelectionFilter no selection filter Curves curves Edges edges Faces faces Feature feature SolidBodies solid bodies SheetBodies sheet bodies FacetBodies facet bodies Groups groups SurfaceRegionFeatures surface region features -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-