NcmHoleMachiningEngRet Class¶
-
class
NXOpen.CAM.
NcmHoleMachiningEngRet
¶ Bases:
NXOpen.TaggedObject
Represents a builder for an inheritable double value in of a CAM.
CAMObject .. versionadded:: NX7.5.0
Properties¶
Property | Description |
---|---|
EngRetType | Returns or sets the type of engage/retract |
Height | Returns the engage/retract height builder |
MinClearance | Returns the engage/retract min clearance builder |
StartFromCenter | Returns or sets the engage/retract start at arc center |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
NcmHoleMachiningEngRetEngRetTypes Enumeration | Available types for engage/retract in Planar Milling |
Property Detail¶
EngRetType¶
-
NcmHoleMachiningEngRet.
EngRetType
¶ Returns or sets the type of engage/retract
-------------------------------------
Getter Method
Signature
EngRetType
Returns: the current value Return type: NXOpen.CAM.NcmHoleMachiningEngRetEngRetTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EngRetType
Parameters: engRetType ( NXOpen.CAM.NcmHoleMachiningEngRetEngRetTypes
) – the new valueNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
Height¶
-
NcmHoleMachiningEngRet.
Height
¶ Returns the engage/retract height builder
-------------------------------------
Getter Method
Signature
Height
Returns: The component builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.5.0.
License requirements: None.
MinClearance¶
-
NcmHoleMachiningEngRet.
MinClearance
¶ Returns the engage/retract min clearance builder
-------------------------------------
Getter Method
Signature
MinClearance
Returns: The component builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX7.5.0.
License requirements: None.
StartFromCenter¶
-
NcmHoleMachiningEngRet.
StartFromCenter
¶ Returns or sets the engage/retract start at arc center
-------------------------------------
Getter Method
Signature
StartFromCenter
Returns: the start from center Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartFromCenter
Parameters: startFromCenter (bool) – the start from center New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)