NcmHoleMachiningEngRetEngRetTypes Enumeration¶
NXOpen.CAM.NcmHoleMachiningEngRet.EngRetTypes is an alias for NXOpen.CAM.NcmHoleMachiningEngRetEngRetTypes
-
class
NXOpen.CAM.
NcmHoleMachiningEngRetEngRetTypes
¶ Bases:
object
Available types for engage/retract in Planar Milling
Enum Members
Enum Member Enum Member Description SameAsDefault Same as Default (Inherit) SameAsEngage Same as Engage Helical Helical Linear Linear Circular Circular NotSet None MinimumClearance Minimum Clearance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-