MachineTurretGroupBuilder Class¶
-
class
NXOpen.CAM.
MachineTurretGroupBuilder
¶ Bases:
NXOpen.CAM.NCGroupBuilder
Represents a MachineTurretGroup Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateMachineTurretGroupBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CarrierName | Returns the Carrier Name object(inheritable text) |
ChannelName | Returns or sets the channel’s name |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
MctTurrentId | Returns or sets the Mct Turrent ID |
MctTurrentWpl | Returns or sets the mct turrent workplane |
MctTurrentWplType | Returns or sets the workplane type |
OptimizationMethod | Returns or sets the optim method |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MachineTurretGroupBuilderMctTurrentWplTypes Enumeration | WorkPlane Type |
Property Detail¶
CarrierName¶
-
MachineTurretGroupBuilder.
CarrierName
¶ Returns the Carrier Name object(inheritable text)
-------------------------------------
Getter Method
Signature
CarrierName
Returns: Return type: NXOpen.CAM.InheritableTextBuilder
New in version NX6.0.0.
License requirements: None.
ChannelName¶
-
MachineTurretGroupBuilder.
ChannelName
¶ Returns or sets the channel’s name
-------------------------------------
Getter Method
Signature
ChannelName
Returns: The channel’s name Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChannelName
Parameters: name (str) – the channel’s name New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
MctTurrentId¶
-
MachineTurretGroupBuilder.
MctTurrentId
¶ Returns or sets the Mct Turrent ID
-------------------------------------
Getter Method
Signature
MctTurrentId
Returns: the mct turrent id value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MctTurrentId
Parameters: mctTurrentID (str) – the mct turrent id value New in version NX5.0.0.
License requirements: None.
MctTurrentWpl¶
-
MachineTurretGroupBuilder.
MctTurrentWpl
¶ Returns or sets the mct turrent workplane
-------------------------------------
Getter Method
Signature
MctTurrentWpl
Returns: the mct turrent wpl value Return type: NXOpen.CartesianCoordinateSystem
New in version NX5.0.0.
Deprecated since version NX9.0.0: None
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Setter Method
Signature
MctTurrentWpl
Parameters: mctTurrentWpl ( NXOpen.CartesianCoordinateSystem
) – the mct turrent wpl valueNew in version NX5.0.0.
Deprecated since version NX9.0.0: None
License requirements: cam_base (“CAM BASE”)
MctTurrentWplType¶
-
MachineTurretGroupBuilder.
MctTurrentWplType
¶ Returns or sets the workplane type
-------------------------------------
Getter Method
Signature
MctTurrentWplType
Returns: Return type: NXOpen.CAM.MachineTurretGroupBuilderMctTurrentWplTypes
New in version NX5.0.0.
Deprecated since version NX9.0.0: None
License requirements: None.
-------------------------------------
Setter Method
Signature
MctTurrentWplType
Parameters: mctTurrentWplType ( NXOpen.CAM.MachineTurretGroupBuilderMctTurrentWplTypes
) –New in version NX5.0.0.
Deprecated since version NX9.0.0: None
License requirements: None.
Method Detail¶
Validate¶
-
MachineTurretGroupBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.