InheritableTextBuilder Class¶
-
class
NXOpen.CAM.
InheritableTextBuilder
¶ Bases:
NXOpen.CAM.InheritableBuilder
Represents a builder for an inheritable text value in of a CAM.
CAMObject .. versionadded:: NX5.0.0
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Tag | Returns the Tag for this object. |
Value | Returns or sets the current value |
Methods¶
Property Detail¶
Value¶
-
InheritableTextBuilder.
Value
¶ Returns or sets the current value
-------------------------------------
Getter Method
Signature
Value
Returns: the current value Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value
Parameters: newValue (str) – the new value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)