InspectionCmmCommandBuilder Class¶
-
class
NXOpen.CAM.
InspectionCmmCommandBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection miscellaneous command builder.
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionCmmCommandBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AngularPlaces | Returns or sets the angular decimal places |
AngularUnits | Returns or sets the angular units |
AutoToggle | Returns or sets the auto mode toggle |
ChannelName | Returns or sets the channel’s name |
CommandType | Returns or sets the command type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
DevTolPlaces | Returns or sets the deviation and tolerance decimal places |
DeviceName | Returns or sets the device name |
DeviceType | Returns or sets the device type |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GotoAangle | Returns or sets the goto A angle |
GotoBangle | Returns or sets the goto B angle |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
HomePtMethod | Returns or sets the home point method |
HomePtPoint | Returns or sets the home point location |
HumidityPlaces | Returns or sets the humidity decimal places |
IdName | Returns or sets the ID name |
IdnameMethod | Returns or sets the ID name method |
IndexSize | Returns or sets the index size |
IntermediatePoint | Returns or sets the intermediate point |
JumpLabel | Returns or sets the program jump label |
LayoutAndLayer | Returns the Layer and Layout |
LinearPlaces | Returns or sets the linear decimal places |
LinearUnits | Returns or sets the linear units |
ManualToggle | Returns or sets the manual mode toggle |
MaxToggle | Returns or sets the max toggle |
MaxValue | Returns or sets the max value |
MinToggle | Returns or sets the min toggle |
MinValue | Returns or sets the min value |
MotionOutputBuilder | Returns the motion output builder |
MoveType | Returns or sets the move type |
Notes | Returns the notes builder |
NumChar | Returns or sets the number of characters |
OpName | Returns or sets the command operation name |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ProgramName | Returns or sets the program name |
ProgramNameMethod | Returns or sets the program name method |
ProgramToggle | Returns or sets the program mode toggle |
PromptVar | Returns or sets the prompt variable |
QisvarType | Returns or sets the qis variable type |
QisvarValue | Returns or sets the qis variable value |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RevMethod | Returns or sets the revision method |
RevName | Returns or sets the revision name |
SafeClearance | Returns the safe clearance builder |
SaveDmlDidLabel | Returns or sets the save DML DID label |
SaveDmlPcsLabel | Returns or sets the save DML PCS label |
SaveDmlPointData | Returns or sets the save DML point data |
SaveDmlVersion | Returns or sets the save DML version |
SelectToolFlag | Returns or sets the user selected tool |
SensorName | Returns or sets the sensor name |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TargetPoint | Returns or sets the target point |
TemperaturePlaces | Returns or sets the temperature decimal places |
TemperatureUnits | Returns or sets the temperature units |
ToolChangeSetting | Returns the tool change builder |
ToolName | Returns or sets the tool name |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
UserPrompt | Returns or sets the user prompt |
VarName | Returns or sets the variable name |
VarScope | Returns or sets the variable scope |
VarType | Returns or sets the variable type |
VectorPlaces | Returns or sets the vector decimal places |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
GetProgStatements | Returns the program statements |
SetHoleAxisValues | Set the Hole Axis values |
SetProgStatements | Sets the program statements |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AngularPlaces¶
-
InspectionCmmCommandBuilder.
AngularPlaces
¶ Returns or sets the angular decimal places
-------------------------------------
Getter Method
Signature
AngularPlaces
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularPlaces
Parameters: angularPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AngularUnits¶
-
InspectionCmmCommandBuilder.
AngularUnits
¶ Returns or sets the angular units
-------------------------------------
Getter Method
Signature
AngularUnits
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderAngularUnitsOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularUnits
Parameters: angularUnits ( NXOpen.CAM.InspectionCmmCommandBuilderAngularUnitsOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AutoToggle¶
-
InspectionCmmCommandBuilder.
AutoToggle
¶ Returns or sets the auto mode toggle
-------------------------------------
Getter Method
Signature
AutoToggle
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutoToggle
Parameters: autoToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CommandType¶
-
InspectionCmmCommandBuilder.
CommandType
¶ Returns or sets the command type
-------------------------------------
Getter Method
Signature
CommandType
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderCommandTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CommandType
Parameters: commandType ( NXOpen.CAM.InspectionCmmCommandBuilderCommandTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DevTolPlaces¶
-
InspectionCmmCommandBuilder.
DevTolPlaces
¶ Returns or sets the deviation and tolerance decimal places
-------------------------------------
Getter Method
Signature
DevTolPlaces
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DevTolPlaces
Parameters: devTolPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DeviceName¶
-
InspectionCmmCommandBuilder.
DeviceName
¶ Returns or sets the device name
-------------------------------------
Getter Method
Signature
DeviceName
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeviceName
Parameters: deviceName (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DeviceType¶
-
InspectionCmmCommandBuilder.
DeviceType
¶ Returns or sets the device type
-------------------------------------
Getter Method
Signature
DeviceType
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderDeviceTypeOptions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DeviceType
Parameters: deviceType ( NXOpen.CAM.InspectionCmmCommandBuilderDeviceTypeOptions
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
GotoAangle¶
-
InspectionCmmCommandBuilder.
GotoAangle
¶ Returns or sets the goto A angle
-------------------------------------
Getter Method
Signature
GotoAangle
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GotoAangle
Parameters: gotoAangle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
GotoBangle¶
-
InspectionCmmCommandBuilder.
GotoBangle
¶ Returns or sets the goto B angle
-------------------------------------
Getter Method
Signature
GotoBangle
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GotoBangle
Parameters: gotoBangle (float) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
HomePtMethod¶
-
InspectionCmmCommandBuilder.
HomePtMethod
¶ Returns or sets the home point method
-------------------------------------
Getter Method
Signature
HomePtMethod
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderHomePtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HomePtMethod
Parameters: homePtMethod ( NXOpen.CAM.InspectionCmmCommandBuilderHomePtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
HomePtPoint¶
-
InspectionCmmCommandBuilder.
HomePtPoint
¶ Returns or sets the home point location
-------------------------------------
Getter Method
Signature
HomePtPoint
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HomePtPoint
Parameters: homePtPoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
HumidityPlaces¶
-
InspectionCmmCommandBuilder.
HumidityPlaces
¶ Returns or sets the humidity decimal places
-------------------------------------
Getter Method
Signature
HumidityPlaces
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HumidityPlaces
Parameters: humidityPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IdName¶
-
InspectionCmmCommandBuilder.
IdName
¶ Returns or sets the ID name
-------------------------------------
Getter Method
Signature
IdName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdName
Parameters: idName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IdnameMethod¶
-
InspectionCmmCommandBuilder.
IdnameMethod
¶ Returns or sets the ID name method
-------------------------------------
Getter Method
Signature
IdnameMethod
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderIdnameMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdnameMethod
Parameters: idnameMethod ( NXOpen.CAM.InspectionCmmCommandBuilderIdnameMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IndexSize¶
-
InspectionCmmCommandBuilder.
IndexSize
¶ Returns or sets the index size
-------------------------------------
Getter Method
Signature
IndexSize
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IndexSize
Parameters: indexSize (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IntermediatePoint¶
-
InspectionCmmCommandBuilder.
IntermediatePoint
¶ Returns or sets the intermediate point
-------------------------------------
Getter Method
Signature
IntermediatePoint
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IntermediatePoint
Parameters: intermediatePoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
JumpLabel¶
-
InspectionCmmCommandBuilder.
JumpLabel
¶ Returns or sets the program jump label
-------------------------------------
Getter Method
Signature
JumpLabel
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JumpLabel
Parameters: jumpLabel (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LinearPlaces¶
-
InspectionCmmCommandBuilder.
LinearPlaces
¶ Returns or sets the linear decimal places
-------------------------------------
Getter Method
Signature
LinearPlaces
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearPlaces
Parameters: linearPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LinearUnits¶
-
InspectionCmmCommandBuilder.
LinearUnits
¶ Returns or sets the linear units
-------------------------------------
Getter Method
Signature
LinearUnits
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderLinearUnitsOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinearUnits
Parameters: linearUnits ( NXOpen.CAM.InspectionCmmCommandBuilderLinearUnitsOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ManualToggle¶
-
InspectionCmmCommandBuilder.
ManualToggle
¶ Returns or sets the manual mode toggle
-------------------------------------
Getter Method
Signature
ManualToggle
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ManualToggle
Parameters: manualToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaxToggle¶
-
InspectionCmmCommandBuilder.
MaxToggle
¶ Returns or sets the max toggle
-------------------------------------
Getter Method
Signature
MaxToggle
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxToggle
Parameters: maxToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaxValue¶
-
InspectionCmmCommandBuilder.
MaxValue
¶ Returns or sets the max value
-------------------------------------
Getter Method
Signature
MaxValue
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxValue
Parameters: maxValue (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinToggle¶
-
InspectionCmmCommandBuilder.
MinToggle
¶ Returns or sets the min toggle
-------------------------------------
Getter Method
Signature
MinToggle
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinToggle
Parameters: minToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinValue¶
-
InspectionCmmCommandBuilder.
MinValue
¶ Returns or sets the min value
-------------------------------------
Getter Method
Signature
MinValue
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinValue
Parameters: minValue (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MoveType¶
-
InspectionCmmCommandBuilder.
MoveType
¶ Returns or sets the move type
-------------------------------------
Getter Method
Signature
MoveType
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderMoveTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MoveType
Parameters: moveType ( NXOpen.CAM.InspectionCmmCommandBuilderMoveTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
NumChar¶
-
InspectionCmmCommandBuilder.
NumChar
¶ Returns or sets the number of characters
-------------------------------------
Getter Method
Signature
NumChar
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumChar
Parameters: numChar (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OpName¶
-
InspectionCmmCommandBuilder.
OpName
¶ Returns or sets the command operation name
-------------------------------------
Getter Method
Signature
OpName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OpName
Parameters: opName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProgramName¶
-
InspectionCmmCommandBuilder.
ProgramName
¶ Returns or sets the program name
-------------------------------------
Getter Method
Signature
ProgramName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramName
Parameters: programName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProgramNameMethod¶
-
InspectionCmmCommandBuilder.
ProgramNameMethod
¶ Returns or sets the program name method
-------------------------------------
Getter Method
Signature
ProgramNameMethod
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderProgramNameMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramNameMethod
Parameters: programNameMethod ( NXOpen.CAM.InspectionCmmCommandBuilderProgramNameMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ProgramToggle¶
-
InspectionCmmCommandBuilder.
ProgramToggle
¶ Returns or sets the program mode toggle
-------------------------------------
Getter Method
Signature
ProgramToggle
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProgramToggle
Parameters: programToggle (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PromptVar¶
-
InspectionCmmCommandBuilder.
PromptVar
¶ Returns or sets the prompt variable
-------------------------------------
Getter Method
Signature
PromptVar
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderPromptVars
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PromptVar
Parameters: promptVar ( NXOpen.CAM.InspectionCmmCommandBuilderPromptVars
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
QisvarType¶
-
InspectionCmmCommandBuilder.
QisvarType
¶ Returns or sets the qis variable type
-------------------------------------
Getter Method
Signature
QisvarType
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderQisvarTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QisvarType
Parameters: qisvarType ( NXOpen.CAM.InspectionCmmCommandBuilderQisvarTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
QisvarValue¶
-
InspectionCmmCommandBuilder.
QisvarValue
¶ Returns or sets the qis variable value
-------------------------------------
Getter Method
Signature
QisvarValue
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
QisvarValue
Parameters: qisvarValue (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RevMethod¶
-
InspectionCmmCommandBuilder.
RevMethod
¶ Returns or sets the revision method
-------------------------------------
Getter Method
Signature
RevMethod
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderRevMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RevMethod
Parameters: revMethod ( NXOpen.CAM.InspectionCmmCommandBuilderRevMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RevName¶
-
InspectionCmmCommandBuilder.
RevName
¶ Returns or sets the revision name
-------------------------------------
Getter Method
Signature
RevName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RevName
Parameters: revName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlDidLabel¶
-
InspectionCmmCommandBuilder.
SaveDmlDidLabel
¶ Returns or sets the save DML DID label
-------------------------------------
Getter Method
Signature
SaveDmlDidLabel
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlDidLabel
Parameters: saveDmlDidLabel (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlPcsLabel¶
-
InspectionCmmCommandBuilder.
SaveDmlPcsLabel
¶ Returns or sets the save DML PCS label
-------------------------------------
Getter Method
Signature
SaveDmlPcsLabel
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlPcsLabel
Parameters: savePcsDidLabel (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlPointData¶
-
InspectionCmmCommandBuilder.
SaveDmlPointData
¶ Returns or sets the save DML point data
-------------------------------------
Getter Method
Signature
SaveDmlPointData
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlPointData
Parameters: saveDmlPointData (bool) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDmlVersion¶
-
InspectionCmmCommandBuilder.
SaveDmlVersion
¶ Returns or sets the save DML version
-------------------------------------
Getter Method
Signature
SaveDmlVersion
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDmlVersion
Parameters: saveDmlVersion (str) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SensorName¶
-
InspectionCmmCommandBuilder.
SensorName
¶ Returns or sets the sensor name
-------------------------------------
Getter Method
Signature
SensorName
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SensorName
Parameters: sensorName (str) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TargetPoint¶
-
InspectionCmmCommandBuilder.
TargetPoint
¶ Returns or sets the target point
-------------------------------------
Getter Method
Signature
TargetPoint
Returns: Return type: NXOpen.Point
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetPoint
Parameters: targetPoint ( NXOpen.Point
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TemperaturePlaces¶
-
InspectionCmmCommandBuilder.
TemperaturePlaces
¶ Returns or sets the temperature decimal places
-------------------------------------
Getter Method
Signature
TemperaturePlaces
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemperaturePlaces
Parameters: temperaturePlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TemperatureUnits¶
-
InspectionCmmCommandBuilder.
TemperatureUnits
¶ Returns or sets the temperature units
-------------------------------------
Getter Method
Signature
TemperatureUnits
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderTemperatureUnitsOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TemperatureUnits
Parameters: temperatureUnits ( NXOpen.CAM.InspectionCmmCommandBuilderTemperatureUnitsOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ToolName¶
-
InspectionCmmCommandBuilder.
ToolName
¶ Returns or sets the tool name
-------------------------------------
Getter Method
Signature
ToolName
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolName
Parameters: toolName (str) – New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UserPrompt¶
-
InspectionCmmCommandBuilder.
UserPrompt
¶ Returns or sets the user prompt
-------------------------------------
Getter Method
Signature
UserPrompt
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserPrompt
Parameters: userPrompt (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VarName¶
-
InspectionCmmCommandBuilder.
VarName
¶ Returns or sets the variable name
-------------------------------------
Getter Method
Signature
VarName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VarName
Parameters: varName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VarScope¶
-
InspectionCmmCommandBuilder.
VarScope
¶ Returns or sets the variable scope
-------------------------------------
Getter Method
Signature
VarScope
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderVarScopes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VarScope
Parameters: varScope ( NXOpen.CAM.InspectionCmmCommandBuilderVarScopes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VarType¶
-
InspectionCmmCommandBuilder.
VarType
¶ Returns or sets the variable type
-------------------------------------
Getter Method
Signature
VarType
Returns: Return type: NXOpen.CAM.InspectionCmmCommandBuilderVarTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VarType
Parameters: varType ( NXOpen.CAM.InspectionCmmCommandBuilderVarTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
VectorPlaces¶
-
InspectionCmmCommandBuilder.
VectorPlaces
¶ Returns or sets the vector decimal places
-------------------------------------
Getter Method
Signature
VectorPlaces
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorPlaces
Parameters: vectorPlaces (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetProgStatements¶
-
InspectionCmmCommandBuilder.
GetProgStatements
¶ Returns the program statements
Signature
GetProgStatements()
Returns: Return type: list of str New in version NX7.0.0.
License requirements: None.
SetProgStatements¶
-
InspectionCmmCommandBuilder.
SetProgStatements
¶ Sets the program statements
Signature
SetProgStatements(progStatements)
Parameters: progStatements (list of str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionCmmCommandBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.