InspectionCmmCommandBuilderCommandTypes Enumeration¶
NXOpen.CAM.InspectionCmmCommandBuilder.CommandTypes is an alias for NXOpen.CAM.InspectionCmmCommandBuilderCommandTypes
-
class
NXOpen.CAM.
InspectionCmmCommandBuilderCommandTypes
¶ Bases:
object
The type of CMM command to be entered
Enum Members
Enum Member Enum Member Description EnterStatement Enter any CMM statement MeasurementMode Enter a statement to set the measurement mode DefineHomePoint Enter a statement defining the home point MoveMachine Enter a statement to move the machine OutputDecimalPlaces Enter a statement defining the number of decimal places for output DeclareVariable Enter a statement declaring a variable QISVariable Enter a statement declaring a QIS variable PromptforInput Enter a statement prompting the user for input ProgramLabel Enter a program label statement JumptoLabel Enter a jump to label statement ProgramHeader Enter a program header statement SensorSelect Enter a statement defining a sensor selection statement Device Enter a statement defining a device statement SaveDml Enter a statement defining a Save DML statement -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-