InspectionCmmCommandBuilderVarTypes Enumeration¶
NXOpen.CAM.InspectionCmmCommandBuilder.VarTypes is an alias for NXOpen.CAM.InspectionCmmCommandBuilderVarTypes
-
class
NXOpen.CAM.
InspectionCmmCommandBuilderVarTypes
¶ Bases:
object
Variable type
Enum Members
Enum Member Enum Member Description Boolean Specifies a boolean variable Integer Specifies an integer variable Long Specifies a long integer variable Real Specifies a real variable Double Specifies a double variable Character Specifies a character variable Vector Specifies a vector variable -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-