InspectionAlignmentBuilder Class¶
-
class
NXOpen.CAM.
InspectionAlignmentBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Alignment builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionAlignmentBuilder()
New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
AlignOpName | Returns or sets the align op name |
AlignType | Returns or sets the alignment type |
ChannelName | Returns or sets the channel’s name |
ComponentSelection | Returns the component selection |
CsysPick | Returns or sets the csys pick |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FailGroupName | Returns or sets the fail group name |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
IterAvailSelect | Returns the iter avail select |
IterConvergeVar | Returns or sets the iter converge variable |
IterDev | Returns or sets the iter deviation |
IterDevType | Returns or sets the iter deviation type |
IterGroupName | Returns or sets the iter group name |
IterMax | Returns or sets the iter max iterations |
LayoutAndLayer | Returns the Layer and Layout |
LocateAvailSelect | Returns the locate avail select |
LocateXrot | Returns or sets the locate xrot |
LocateXtrans | Returns or sets the locate xtrans |
LocateYrot | Returns or sets the locate yrot |
LocateYtrans | Returns or sets the locate ytrans |
LocateZrot | Returns or sets the locate zrot |
LocateZtrans | Returns or sets the locate ztrans |
MotionOutputBuilder | Returns the motion output builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PcsName | Returns or sets the pcs name |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
PriDatLetter | Returns or sets the pri dat letter |
PriDirection | Returns or sets the pri direction |
PriXorigin | Returns or sets the pri xorigin |
PriYorigin | Returns or sets the pri yorigin |
PriZorigin | Returns or sets the pri zorigin |
RPSAvailSelect | Returns the RPS available select |
RecallCsys | Returns or sets the recall csys |
RecallDid | Returns or sets the recall device id |
RecallExtName | Returns or sets the recall external name |
RecallIntName | Returns or sets the recall internal name |
RecallState | Returns or sets the recall state |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
RotateTableAngle | Returns or sets the angle to rotate table |
RotateTableAngularDeviation | Returns or sets the rotate table angular deviation |
RotateTableDirection | Returns or sets the rotate table direction |
RotateTableFeature | Returns or sets the feature used to position table |
RotateTableFeatureSelect | Returns the feature selected to position table |
RotateTableMethod | Returns or sets the rotate table method |
RotateTableName | Returns or sets the name of rotary table to rotate |
RotateTablePcsUpdateOption | Returns or sets the rotate table pcs update |
RotationAngle | Returns or sets the rot angle |
RotationAxis | Returns or sets the rot axis |
RotationDatumLetter | Returns or sets the rot datum letter |
RotationDirection | Returns or sets the rot dir |
RotationFeature | Returns or sets the rot feature |
RotationFeatureSelect | Returns the rot feature select |
RotationMethod | Returns or sets the rot method |
SafeClearance | Returns the safe clearance builder |
SaveDid | Returns or sets the save device id |
SavePcsLabel | Returns or sets the save pcs label |
SaveState | Returns or sets the save state |
SecDatLetter | Returns or sets the sec dat letter |
SecDirection | Returns or sets the sec direction |
SecXorigin | Returns or sets the sec xorigin |
SecYorigin | Returns or sets the sec yorigin |
SecZorigin | Returns or sets the sec zorigin |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TerDatLetter | Returns or sets the ter dat letter |
TerDirection | Returns or sets the ter xdirection |
TerXorigin | Returns or sets the ter xorigin |
TerYorigin | Returns or sets the ter yorigin |
TerZorigin | Returns or sets the ter zorigin |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
WcsOrientOption | Returns or sets the WCS Orient option |
XtDatumLetter | Returns or sets the xt datum letter |
XtDistance | Returns or sets the xt distance |
XtFeature | Returns or sets the xt feature |
XtFeatureSelect | Returns the xt feature select |
XtMethod | Returns or sets the xt method |
YtDatumLetter | Returns or sets the yt datum letter |
YtDistance | Returns or sets the yt distance |
YtFeature | Returns or sets the yt feature |
YtFeatureSelect | Returns the yt feature select |
YtMethod | Returns or sets the yt method |
ZtDatumLetter | Returns or sets the zt datum letter |
ZtDistance | Returns or sets the zt distance |
ZtFeature | Returns or sets the zt feature |
ZtFeatureSelect | Returns the zt feature select |
ZtMethod | Returns or sets the zt method |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetHoleAxisValues | Get the Hole Axis values |
GetLocateFeatures | Return the Locate features. |
GetObject | Returns the object currently being edited by this builder. |
GetRPSFeatures | Return the RPS features. |
GetRPSXFeatures | Return the RPS features controlling the X direction. |
GetRPSYFeatures | Return the RPS features controlling the Y direction. |
GetRPSZFeatures | Return the RPS features controlling the Z direction. |
SetHoleAxisValues | Set the Hole Axis values |
SetLocateFeatures | Set the Locate features. |
SetRPSFeatures | Set the RPS features. |
SetRPSXFeatures | Set the RPS features controlling the X direction. |
SetRPSYFeatures | Set the RPS features controlling the Y direction. |
SetRPSZFeatures | Set the RPS features controlling the Z direction. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AlignOpName¶
-
InspectionAlignmentBuilder.
AlignOpName
¶ Returns or sets the align op name
-------------------------------------
Getter Method
Signature
AlignOpName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignOpName
Parameters: alignOpName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
AlignType¶
-
InspectionAlignmentBuilder.
AlignType
¶ Returns or sets the alignment type
-------------------------------------
Getter Method
Signature
AlignType
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlignType
Parameters: alignType ( NXOpen.CAM.InspectionAlignmentBuilderAlignTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ComponentSelection¶
-
InspectionAlignmentBuilder.
ComponentSelection
¶ Returns the component selection
-------------------------------------
Getter Method
Signature
ComponentSelection
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX9.0.0.
License requirements: None.
CsysPick¶
-
InspectionAlignmentBuilder.
CsysPick
¶ Returns or sets the csys pick
-------------------------------------
Getter Method
Signature
CsysPick
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysPick
Parameters: csysPick ( NXOpen.CoordinateSystem
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
FailGroupName¶
-
InspectionAlignmentBuilder.
FailGroupName
¶ Returns or sets the fail group name
-------------------------------------
Getter Method
Signature
FailGroupName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FailGroupName
Parameters: failGroupName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterAvailSelect¶
-
InspectionAlignmentBuilder.
IterAvailSelect
¶ Returns the iter avail select
-------------------------------------
Getter Method
Signature
IterAvailSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
IterConvergeVar¶
-
InspectionAlignmentBuilder.
IterConvergeVar
¶ Returns or sets the iter converge variable
-------------------------------------
Getter Method
Signature
IterConvergeVar
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterConvergeVar
Parameters: iterConvergeVar (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterDev¶
-
InspectionAlignmentBuilder.
IterDev
¶ Returns or sets the iter deviation
-------------------------------------
Getter Method
Signature
IterDev
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterDev
Parameters: iterDev (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterDevType¶
-
InspectionAlignmentBuilder.
IterDevType
¶ Returns or sets the iter deviation type
-------------------------------------
Getter Method
Signature
IterDevType
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderIterDevTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterDevType
Parameters: iterDevType ( NXOpen.CAM.InspectionAlignmentBuilderIterDevTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterGroupName¶
-
InspectionAlignmentBuilder.
IterGroupName
¶ Returns or sets the iter group name
-------------------------------------
Getter Method
Signature
IterGroupName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterGroupName
Parameters: iterGroupName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IterMax¶
-
InspectionAlignmentBuilder.
IterMax
¶ Returns or sets the iter max iterations
-------------------------------------
Getter Method
Signature
IterMax
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IterMax
Parameters: iterMax (int) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateAvailSelect¶
-
InspectionAlignmentBuilder.
LocateAvailSelect
¶ Returns the locate avail select
-------------------------------------
Getter Method
Signature
LocateAvailSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
LocateXrot¶
-
InspectionAlignmentBuilder.
LocateXrot
¶ Returns or sets the locate xrot
-------------------------------------
Getter Method
Signature
LocateXrot
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateXrot
Parameters: locateXrot (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateXtrans¶
-
InspectionAlignmentBuilder.
LocateXtrans
¶ Returns or sets the locate xtrans
-------------------------------------
Getter Method
Signature
LocateXtrans
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateXtrans
Parameters: locateXtrans (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateYrot¶
-
InspectionAlignmentBuilder.
LocateYrot
¶ Returns or sets the locate yrot
-------------------------------------
Getter Method
Signature
LocateYrot
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateYrot
Parameters: locateYrot (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateYtrans¶
-
InspectionAlignmentBuilder.
LocateYtrans
¶ Returns or sets the locate ytrans
-------------------------------------
Getter Method
Signature
LocateYtrans
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateYtrans
Parameters: locateYtrans (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateZrot¶
-
InspectionAlignmentBuilder.
LocateZrot
¶ Returns or sets the locate zrot
-------------------------------------
Getter Method
Signature
LocateZrot
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateZrot
Parameters: locateZrot (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
LocateZtrans¶
-
InspectionAlignmentBuilder.
LocateZtrans
¶ Returns or sets the locate ztrans
-------------------------------------
Getter Method
Signature
LocateZtrans
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LocateZtrans
Parameters: locateZtrans (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PcsName¶
-
InspectionAlignmentBuilder.
PcsName
¶ Returns or sets the pcs name
-------------------------------------
Getter Method
Signature
PcsName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PcsName
Parameters: pcsName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriDatLetter¶
-
InspectionAlignmentBuilder.
PriDatLetter
¶ Returns or sets the pri dat letter
-------------------------------------
Getter Method
Signature
PriDatLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriDatLetter
Parameters: priDatLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriDirection¶
-
InspectionAlignmentBuilder.
PriDirection
¶ Returns or sets the pri direction
-------------------------------------
Getter Method
Signature
PriDirection
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriDirection
Parameters: priDirection ( NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriXorigin¶
-
InspectionAlignmentBuilder.
PriXorigin
¶ Returns or sets the pri xorigin
-------------------------------------
Getter Method
Signature
PriXorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriXorigin
Parameters: priXorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriYorigin¶
-
InspectionAlignmentBuilder.
PriYorigin
¶ Returns or sets the pri yorigin
-------------------------------------
Getter Method
Signature
PriYorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriYorigin
Parameters: priYorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PriZorigin¶
-
InspectionAlignmentBuilder.
PriZorigin
¶ Returns or sets the pri zorigin
-------------------------------------
Getter Method
Signature
PriZorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PriZorigin
Parameters: priZorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RPSAvailSelect¶
-
InspectionAlignmentBuilder.
RPSAvailSelect
¶ Returns the RPS available select
-------------------------------------
Getter Method
Signature
RPSAvailSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX11.0.1.
License requirements: None.
RecallCsys¶
-
InspectionAlignmentBuilder.
RecallCsys
¶ Returns or sets the recall csys
-------------------------------------
Getter Method
Signature
RecallCsys
Returns: Return type: NXOpen.CoordinateSystem
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallCsys
Parameters: recallCsys ( NXOpen.CoordinateSystem
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallDid¶
-
InspectionAlignmentBuilder.
RecallDid
¶ Returns or sets the recall device id
-------------------------------------
Getter Method
Signature
RecallDid
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallDid
Parameters: recallDid (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallExtName¶
-
InspectionAlignmentBuilder.
RecallExtName
¶ Returns or sets the recall external name
-------------------------------------
Getter Method
Signature
RecallExtName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallExtName
Parameters: recallExtName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallIntName¶
-
InspectionAlignmentBuilder.
RecallIntName
¶ Returns or sets the recall internal name
-------------------------------------
Getter Method
Signature
RecallIntName
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallIntName
Parameters: recallIntName (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RecallState¶
-
InspectionAlignmentBuilder.
RecallState
¶ Returns or sets the recall state
-------------------------------------
Getter Method
Signature
RecallState
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRecallStates
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RecallState
Parameters: recallState ( NXOpen.CAM.InspectionAlignmentBuilderRecallStates
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableAngle¶
-
InspectionAlignmentBuilder.
RotateTableAngle
¶ Returns or sets the angle to rotate table
-------------------------------------
Getter Method
Signature
RotateTableAngle
Returns: Return type: float New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableAngle
Parameters: angle (float) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableAngularDeviation¶
-
InspectionAlignmentBuilder.
RotateTableAngularDeviation
¶ Returns or sets the rotate table angular deviation
-------------------------------------
Getter Method
Signature
RotateTableAngularDeviation
Returns: Return type: float New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableAngularDeviation
Parameters: fz (float) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableDirection¶
-
InspectionAlignmentBuilder.
RotateTableDirection
¶ Returns or sets the rotate table direction
-------------------------------------
Getter Method
Signature
RotateTableDirection
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotateTableDirections
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableDirection
Parameters: direction ( NXOpen.CAM.InspectionAlignmentBuilderRotateTableDirections
) –New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableFeature¶
-
InspectionAlignmentBuilder.
RotateTableFeature
¶ Returns or sets the feature used to position table
-------------------------------------
Getter Method
Signature
RotateTableFeature
Returns: Return type: str New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableFeature
Parameters: rotateTableFeature (str) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableFeatureSelect¶
-
InspectionAlignmentBuilder.
RotateTableFeatureSelect
¶ Returns the feature selected to position table
-------------------------------------
Getter Method
Signature
RotateTableFeatureSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.2.
License requirements: None.
RotateTableMethod¶
-
InspectionAlignmentBuilder.
RotateTableMethod
¶ Returns or sets the rotate table method
-------------------------------------
Getter Method
Signature
RotateTableMethod
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotateTableMethods
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableMethod
Parameters: method ( NXOpen.CAM.InspectionAlignmentBuilderRotateTableMethods
) –New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTableName¶
-
InspectionAlignmentBuilder.
RotateTableName
¶ Returns or sets the name of rotary table to rotate
-------------------------------------
Getter Method
Signature
RotateTableName
Returns: Return type: str New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTableName
Parameters: tableName (str) – New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotateTablePcsUpdateOption¶
-
InspectionAlignmentBuilder.
RotateTablePcsUpdateOption
¶ Returns or sets the rotate table pcs update
-------------------------------------
Getter Method
Signature
RotateTablePcsUpdateOption
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotateTablePcsUpdateOptions
New in version NX7.5.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateTablePcsUpdateOption
Parameters: pcsUpdate ( NXOpen.CAM.InspectionAlignmentBuilderRotateTablePcsUpdateOptions
) –New in version NX7.5.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationAngle¶
-
InspectionAlignmentBuilder.
RotationAngle
¶ Returns or sets the rot angle
-------------------------------------
Getter Method
Signature
RotationAngle
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationAngle
Parameters: rotationAngle (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationAxis¶
-
InspectionAlignmentBuilder.
RotationAxis
¶ Returns or sets the rot axis
-------------------------------------
Getter Method
Signature
RotationAxis
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotationAxisOptions
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationAxis
Parameters: rotationAxis ( NXOpen.CAM.InspectionAlignmentBuilderRotationAxisOptions
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationDatumLetter¶
-
InspectionAlignmentBuilder.
RotationDatumLetter
¶ Returns or sets the rot datum letter
-------------------------------------
Getter Method
Signature
RotationDatumLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationDatumLetter
Parameters: rotationDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationDirection¶
-
InspectionAlignmentBuilder.
RotationDirection
¶ Returns or sets the rot dir
-------------------------------------
Getter Method
Signature
RotationDirection
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotationDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationDirection
Parameters: rotationDirection ( NXOpen.CAM.InspectionAlignmentBuilderRotationDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationFeature¶
-
InspectionAlignmentBuilder.
RotationFeature
¶ Returns or sets the rot feature
-------------------------------------
Getter Method
Signature
RotationFeature
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationFeature
Parameters: rotationFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
RotationFeatureSelect¶
-
InspectionAlignmentBuilder.
RotationFeatureSelect
¶ Returns the rot feature select
-------------------------------------
Getter Method
Signature
RotationFeatureSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
RotationMethod¶
-
InspectionAlignmentBuilder.
RotationMethod
¶ Returns or sets the rot method
-------------------------------------
Getter Method
Signature
RotationMethod
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderRotationMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotationMethod
Parameters: rotationMethod ( NXOpen.CAM.InspectionAlignmentBuilderRotationMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveDid¶
-
InspectionAlignmentBuilder.
SaveDid
¶ Returns or sets the save device id
-------------------------------------
Getter Method
Signature
SaveDid
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveDid
Parameters: saveDid (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SavePcsLabel¶
-
InspectionAlignmentBuilder.
SavePcsLabel
¶ Returns or sets the save pcs label
-------------------------------------
Getter Method
Signature
SavePcsLabel
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SavePcsLabel
Parameters: savePcsLabel (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SaveState¶
-
InspectionAlignmentBuilder.
SaveState
¶ Returns or sets the save state
-------------------------------------
Getter Method
Signature
SaveState
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderSaveStates
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveState
Parameters: saveState ( NXOpen.CAM.InspectionAlignmentBuilderSaveStates
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecDatLetter¶
-
InspectionAlignmentBuilder.
SecDatLetter
¶ Returns or sets the sec dat letter
-------------------------------------
Getter Method
Signature
SecDatLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecDatLetter
Parameters: secDatLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecDirection¶
-
InspectionAlignmentBuilder.
SecDirection
¶ Returns or sets the sec direction
-------------------------------------
Getter Method
Signature
SecDirection
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecDirection
Parameters: secDirection ( NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecXorigin¶
-
InspectionAlignmentBuilder.
SecXorigin
¶ Returns or sets the sec xorigin
-------------------------------------
Getter Method
Signature
SecXorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecXorigin
Parameters: secXorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecYorigin¶
-
InspectionAlignmentBuilder.
SecYorigin
¶ Returns or sets the sec yorigin
-------------------------------------
Getter Method
Signature
SecYorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecYorigin
Parameters: secYorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SecZorigin¶
-
InspectionAlignmentBuilder.
SecZorigin
¶ Returns or sets the sec zorigin
-------------------------------------
Getter Method
Signature
SecZorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SecZorigin
Parameters: secZorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerDatLetter¶
-
InspectionAlignmentBuilder.
TerDatLetter
¶ Returns or sets the ter dat letter
-------------------------------------
Getter Method
Signature
TerDatLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerDatLetter
Parameters: terDatLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerDirection¶
-
InspectionAlignmentBuilder.
TerDirection
¶ Returns or sets the ter xdirection
-------------------------------------
Getter Method
Signature
TerDirection
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerDirection
Parameters: terDirection ( NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerXorigin¶
-
InspectionAlignmentBuilder.
TerXorigin
¶ Returns or sets the ter xorigin
-------------------------------------
Getter Method
Signature
TerXorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerXorigin
Parameters: terXorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerYorigin¶
-
InspectionAlignmentBuilder.
TerYorigin
¶ Returns or sets the ter yorigin
-------------------------------------
Getter Method
Signature
TerYorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerYorigin
Parameters: terYorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
TerZorigin¶
-
InspectionAlignmentBuilder.
TerZorigin
¶ Returns or sets the ter zorigin
-------------------------------------
Getter Method
Signature
TerZorigin
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TerZorigin
Parameters: terZorigin (bool) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
WcsOrientOption¶
-
InspectionAlignmentBuilder.
WcsOrientOption
¶ Returns or sets the WCS Orient option
-------------------------------------
Getter Method
Signature
WcsOrientOption
Returns: Return type: bool New in version NX8.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
WcsOrientOption
Parameters: wcsOrientOption (bool) – New in version NX8.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtDatumLetter¶
-
InspectionAlignmentBuilder.
XtDatumLetter
¶ Returns or sets the xt datum letter
-------------------------------------
Getter Method
Signature
XtDatumLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtDatumLetter
Parameters: xtDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtDistance¶
-
InspectionAlignmentBuilder.
XtDistance
¶ Returns or sets the xt distance
-------------------------------------
Getter Method
Signature
XtDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtDistance
Parameters: xtDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtFeature¶
-
InspectionAlignmentBuilder.
XtFeature
¶ Returns or sets the xt feature
-------------------------------------
Getter Method
Signature
XtFeature
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtFeature
Parameters: xtFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
XtFeatureSelect¶
-
InspectionAlignmentBuilder.
XtFeatureSelect
¶ Returns the xt feature select
-------------------------------------
Getter Method
Signature
XtFeatureSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
XtMethod¶
-
InspectionAlignmentBuilder.
XtMethod
¶ Returns or sets the xt method
-------------------------------------
Getter Method
Signature
XtMethod
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderXtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XtMethod
Parameters: xtMethod ( NXOpen.CAM.InspectionAlignmentBuilderXtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtDatumLetter¶
-
InspectionAlignmentBuilder.
YtDatumLetter
¶ Returns or sets the yt datum letter
-------------------------------------
Getter Method
Signature
YtDatumLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtDatumLetter
Parameters: ytDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtDistance¶
-
InspectionAlignmentBuilder.
YtDistance
¶ Returns or sets the yt distance
-------------------------------------
Getter Method
Signature
YtDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtDistance
Parameters: ytDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtFeature¶
-
InspectionAlignmentBuilder.
YtFeature
¶ Returns or sets the yt feature
-------------------------------------
Getter Method
Signature
YtFeature
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtFeature
Parameters: ytFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
YtFeatureSelect¶
-
InspectionAlignmentBuilder.
YtFeatureSelect
¶ Returns the yt feature select
-------------------------------------
Getter Method
Signature
YtFeatureSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
YtMethod¶
-
InspectionAlignmentBuilder.
YtMethod
¶ Returns or sets the yt method
-------------------------------------
Getter Method
Signature
YtMethod
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderYtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YtMethod
Parameters: ytMethod ( NXOpen.CAM.InspectionAlignmentBuilderYtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtDatumLetter¶
-
InspectionAlignmentBuilder.
ZtDatumLetter
¶ Returns or sets the zt datum letter
-------------------------------------
Getter Method
Signature
ZtDatumLetter
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtDatumLetter
Parameters: ztDatumLetter (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtDistance¶
-
InspectionAlignmentBuilder.
ZtDistance
¶ Returns or sets the zt distance
-------------------------------------
Getter Method
Signature
ZtDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtDistance
Parameters: ztDistance (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtFeature¶
-
InspectionAlignmentBuilder.
ZtFeature
¶ Returns or sets the zt feature
-------------------------------------
Getter Method
Signature
ZtFeature
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtFeature
Parameters: ztFeature (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ZtFeatureSelect¶
-
InspectionAlignmentBuilder.
ZtFeatureSelect
¶ Returns the zt feature select
-------------------------------------
Getter Method
Signature
ZtFeatureSelect
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
ZtMethod¶
-
InspectionAlignmentBuilder.
ZtMethod
¶ Returns or sets the zt method
-------------------------------------
Getter Method
Signature
ZtMethod
Returns: Return type: NXOpen.CAM.InspectionAlignmentBuilderZtMethods
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ZtMethod
Parameters: ztMethod ( NXOpen.CAM.InspectionAlignmentBuilderZtMethods
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
GetLocateFeatures¶
-
InspectionAlignmentBuilder.
GetLocateFeatures
¶ Return the Locate features.
Signature
GetLocateFeatures()
Returns: Locate features Return type: list of str New in version NX11.0.2.
License requirements: None.
GetRPSFeatures¶
-
InspectionAlignmentBuilder.
GetRPSFeatures
¶ Return the RPS features.
Signature
GetRPSFeatures()
Returns: RPS features Return type: list of str New in version NX11.0.1.
License requirements: None.
GetRPSXFeatures¶
-
InspectionAlignmentBuilder.
GetRPSXFeatures
¶ Return the RPS features controlling the X direction.
Signature
GetRPSXFeatures()
Returns: RPS X features Return type: list of str New in version NX11.0.1.
License requirements: None.
GetRPSYFeatures¶
-
InspectionAlignmentBuilder.
GetRPSYFeatures
¶ Return the RPS features controlling the Y direction.
Signature
GetRPSYFeatures()
Returns: RPS Y features Return type: list of str New in version NX11.0.1.
License requirements: None.
GetRPSZFeatures¶
-
InspectionAlignmentBuilder.
GetRPSZFeatures
¶ Return the RPS features controlling the Z direction.
Signature
GetRPSZFeatures()
Returns: RPS Z features Return type: list of str New in version NX11.0.1.
License requirements: None.
SetLocateFeatures¶
-
InspectionAlignmentBuilder.
SetLocateFeatures
¶ Set the Locate features.
Signature
SetLocateFeatures(locateFeatures)
Parameters: locateFeatures (list of str) – Locate features New in version NX11.0.2.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetRPSFeatures¶
-
InspectionAlignmentBuilder.
SetRPSFeatures
¶ Set the RPS features.
Signature
SetRPSFeatures(rpsFeatures)
Parameters: rpsFeatures (list of str) – RPS features New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetRPSXFeatures¶
-
InspectionAlignmentBuilder.
SetRPSXFeatures
¶ Set the RPS features controlling the X direction.
Signature
SetRPSXFeatures(rpsXFeatures)
Parameters: rpsXFeatures (list of str) – RPS X features New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetRPSYFeatures¶
-
InspectionAlignmentBuilder.
SetRPSYFeatures
¶ Set the RPS features controlling the Y direction.
Signature
SetRPSYFeatures(rpsYFeatures)
Parameters: rpsYFeatures (list of str) – RPS Y features New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetRPSZFeatures¶
-
InspectionAlignmentBuilder.
SetRPSZFeatures
¶ Set the RPS features controlling the Z direction.
Signature
SetRPSZFeatures(rpsZFeatures)
Parameters: rpsZFeatures (list of str) – RPS Z features New in version NX11.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionAlignmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.