InspectionAlignmentBuilderAlignTypes Enumeration¶
NXOpen.CAM.InspectionAlignmentBuilder.AlignTypes is an alias for NXOpen.CAM.InspectionAlignmentBuilderAlignTypes
-
class
NXOpen.CAM.
InspectionAlignmentBuilderAlignTypes
¶ Bases:
object
Alignment Operation Type
Enum Members
Enum Member Enum Member Description SetPCStoMCS Set the PCS to Machine CS SetPCStoCSYS Set the PCS to a NX Csys TranslatePCSOrigin Translate the PCS RotatePCS Rotate the PCS DefinePCSfromDatums Define the PCS from datums Iterate Iterate a set of features for convergence DefinePCSfromActualDeviations Locate PCS from Features SavePCS Save current PCS RecallPCS Recall previously saved PCS RotateTable Rotate table SetPCStoCADABS Set the PCS to Cadabs Rps RPS alignment type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-