InspectionAlignmentBuilderAlignmentDirections Enumeration¶
NXOpen.CAM.InspectionAlignmentBuilder.AlignmentDirections is an alias for NXOpen.CAM.InspectionAlignmentBuilderAlignmentDirections
-
class
NXOpen.CAM.
InspectionAlignmentBuilderAlignmentDirections
¶ Bases:
object
Alignment directions of datum features
Enum Members
Enum Member Enum Member Description NotSet No alignment direction specified Pxdir Align feature in the positive X direction Pydir Align feature in the positive Y direction Pzdir Align feature in the positive Z direction Mxdir Align feature in the negitive X direction Mydir Align feature in the negitive Y direction Mzdir Align feature in the negitive Z direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-