FeatureGeometry Class¶
-
class
NXOpen.CAM.FBM.
FeatureGeometry
¶ Bases:
NXOpen.CAM.Geometry
Represents a feature geometry builder
This is an abstract class and cannot be instantiated.
New in version NX9.0.1.
Properties¶
Property | Description |
---|---|
GeometryList | Returns the geometry list |
Tag | Returns the Tag for this object. |
Topology | Returns the topology builder |
UseModelDepth | Returns or sets the use model depth flag |
Methods¶
Method | Description |
---|---|
AddFeatureSet | Creates a feature geometry set |
AppendGeometrySet | Append an geometry set with dumb rules |
AppendNamedGeometry | Append named geometry |
CreateFeatureSet | Create a new empty feature editor |
CreateFeatures | Create a series of (in process) features. |
CreateGeometrySet | Create an empty geometry set |
ExpandSets | Expanding the geometry sets |
GetFeatureSet | Get the in process feature editor at the specified index |
GetMachiningArea | Returns the machining area |
InitializeData | Prepare and update geometry data |
PreselectGeometry | Pre-select the wall geometry |
ReloadList | Reload list from parent |
ReorderFeatures | Reorders the features according to a predefined algorithm |
ReorderFeaturesByDirection | Reorders the features according to primary direction |
ReverseFeatures | Reverse the features |
SetDefaultAttribute | Sets a default attribute value |
SetMachiningArea | Change machining area |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FeatureGeometrySequenceDirectionType Enumeration | the direction types |
FeatureGeometrySequencePatternType Enumeration | the pattern types |
FeatureGeometrySortOrder Enumeration | the optimization types |
Property Detail¶
UseModelDepth¶
-
FeatureGeometry.
UseModelDepth
¶ Returns or sets the use model depth flag
-------------------------------------
Getter Method
Signature
UseModelDepth
Returns: the use model depth flag Return type: bool New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseModelDepth
Parameters: flag (bool) – New in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
AddFeatureSet¶
-
FeatureGeometry.
AddFeatureSet
¶ Creates a feature geometry set
Signature
AddFeatureSet(tagMachiningFeature, featureType)
Parameters: - tagMachiningFeature (
NXOpen.CAM.CAMFeature
) – the machining feature - featureType (str) – the in process feature type
Returns: the new in process feature set
Return type: New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
- tagMachiningFeature (
CreateFeatureSet¶
-
FeatureGeometry.
CreateFeatureSet
¶ Create a new empty feature editor
Signature
CreateFeatureSet()
Returns: the new in process feature set Return type: NXOpen.CAM.FBM.FeatureSet
New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
CreateFeatures¶
-
FeatureGeometry.
CreateFeatures
¶ Create a series of (in process) features.
Depending on the input objects feature recognition is performed. When no known features can be recognized, tagged features are created of type featureType
Signature
CreateFeatures(objects, featureType)
Parameters: - objects (list of
NXOpen.NXObject
) – the geometry objects, can also be machining features - featureType (str) – the machining feature type of the implictly created features when feature recognition fails
Returns: Return type: list of
NXOpen.CAM.FBM.Feature
New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
- objects (list of
GetFeatureSet¶
-
FeatureGeometry.
GetFeatureSet
¶ Get the in process feature editor at the specified index
Signature
GetFeatureSet(nIndex)
Parameters: nIndex (int) – the index of the feature set editor Returns: the in process feature set Return type: NXOpen.CAM.FBM.FeatureSet
New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
GetMachiningArea¶
-
FeatureGeometry.
GetMachiningArea
¶ Returns the machining area
Signature
GetMachiningArea()
Returns: the machining area Return type: str New in version NX9.0.2.
License requirements: None.
ReloadList¶
-
FeatureGeometry.
ReloadList
¶ Reload list from parent
Signature
ReloadList()
New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
ReorderFeatures¶
-
FeatureGeometry.
ReorderFeatures
¶ Reorders the features according to a predefined algorithm
Signature
ReorderFeatures(sortType)
Parameters: sortType ( NXOpen.CAM.FBM.FeatureGeometrySortOrder
) –New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
ReorderFeaturesByDirection¶
-
FeatureGeometry.
ReorderFeaturesByDirection
¶ Overloaded method ReorderFeaturesByDirection
ReorderFeaturesByDirection(direction, pattern, vecValue)
ReorderFeaturesByDirection(direction, pattern, vecValue, bandWidth)
-------------------------------------
Reorders the features according to primary direction
Signature
ReorderFeaturesByDirection(direction, pattern, vecValue)
Parameters: - direction (
NXOpen.CAM.FBM.FeatureGeometrySequenceDirectionType
) – - pattern (
NXOpen.CAM.FBM.FeatureGeometrySequencePatternType
) – - vecValue (
NXOpen.Vector3d
) –
New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Reorders the features according to primary direction with band width
Signature
ReorderFeaturesByDirection(direction, pattern, vecValue, bandWidth)
Parameters: - direction (
NXOpen.CAM.FBM.FeatureGeometrySequenceDirectionType
) – - pattern (
NXOpen.CAM.FBM.FeatureGeometrySequencePatternType
) – - vecValue (
NXOpen.Vector3d
) – - bandWidth (float) –
New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
ReverseFeatures¶
-
FeatureGeometry.
ReverseFeatures
¶ Reverse the features
Signature
ReverseFeatures()
New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
SetDefaultAttribute¶
-
FeatureGeometry.
SetDefaultAttribute
¶ Overloaded method SetDefaultAttribute
SetDefaultAttribute(attributeName, dValue)
SetDefaultAttribute(attributeName, strValue)
SetDefaultAttribute(attributeName, nValue)
SetDefaultAttribute(attributeName, bValue)
-------------------------------------
Sets a default attribute value
Signature
SetDefaultAttribute(attributeName, dValue)
Parameters: - attributeName (str) – the attribute name
- dValue (float) – the attribute value
New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Sets a default attribute value
Signature
SetDefaultAttribute(attributeName, strValue)
Parameters: - attributeName (str) – the attribute name
- strValue (str) – the attribute value
New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Sets a default attribute value
Signature
SetDefaultAttribute(attributeName, nValue)
Parameters: - attributeName (str) – the attribute name
- nValue (int) – the attribute value
New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Sets a default attribute value
Signature
SetDefaultAttribute(attributeName, bValue)
Parameters: - attributeName (str) – the attribute name
- bValue (bool) – the attribute value
New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
SetMachiningArea¶
-
FeatureGeometry.
SetMachiningArea
¶ Change machining area
Signature
SetMachiningArea(machiningArea)
Parameters: machiningArea (str) – the machining area New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
FeatureGeometry.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.