FeatureGeometrySequenceDirectionType Enumeration¶
NXOpen.CAM.FBM.FeatureGeometry.SequenceDirectionType is an alias for NXOpen.CAM.FBM.FeatureGeometrySequenceDirectionType
-
class
NXOpen.CAM.FBM.
FeatureGeometrySequenceDirectionType
¶ Bases:
object
the direction types
New in version NX9.0.2.
Enum Members
Enum Member Enum Member Description Xm Direction: XM Ym Direction: YM Zm Direction: ZM Vector Direction: Vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-