BoundaryTurnMemberFineFinishCorner Class¶
-
class
NXOpen.CAM.
BoundaryTurnMemberFineFinishCorner
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.BoundaryTurnMemberFineFinishCorner
This builder cannot be instantiated separately.
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
AngleValue | Returns or sets the fine_finish_corner angle value |
AppliedToType | Returns or sets the fine_finish_corner applied to |
CleanupType | Returns or sets the fine_finish_corner cleanup |
Distance | Returns or sets the fine_finish_corner distance |
Tag | Returns the Tag for this object. |
Type | Returns or sets the fine_finish_corner type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BoundaryTurnMemberFineFinishCornerAppliedTo Enumeration | the corner applied to available |
BoundaryTurnMemberFineFinishCornerCleanup Enumeration | the corner cleanup available |
BoundaryTurnMemberFineFinishCornerValueType Enumeration | the corner types available |
Property Detail¶
AngleValue¶
-
BoundaryTurnMemberFineFinishCorner.
AngleValue
¶ Returns or sets the fine_finish_corner angle value
-------------------------------------
Getter Method
Signature
AngleValue
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleValue
Parameters: cornerAngle (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
AppliedToType¶
-
BoundaryTurnMemberFineFinishCorner.
AppliedToType
¶ Returns or sets the fine_finish_corner applied to
-------------------------------------
Getter Method
Signature
AppliedToType
Returns: Return type: NXOpen.CAM.BoundaryTurnMemberFineFinishCornerAppliedTo
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
AppliedToType
Parameters: appliedTo ( NXOpen.CAM.BoundaryTurnMemberFineFinishCornerAppliedTo
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
CleanupType¶
-
BoundaryTurnMemberFineFinishCorner.
CleanupType
¶ Returns or sets the fine_finish_corner cleanup
-------------------------------------
Getter Method
Signature
CleanupType
Returns: Return type: NXOpen.CAM.BoundaryTurnMemberFineFinishCornerCleanup
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CleanupType
Parameters: cornerCleanup ( NXOpen.CAM.BoundaryTurnMemberFineFinishCornerCleanup
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Distance¶
-
BoundaryTurnMemberFineFinishCorner.
Distance
¶ Returns or sets the fine_finish_corner distance
-------------------------------------
Getter Method
Signature
Distance
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance
Parameters: distance (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Type¶
-
BoundaryTurnMemberFineFinishCorner.
Type
¶ Returns or sets the fine_finish_corner type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.CAM.BoundaryTurnMemberFineFinishCornerValueType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: cornerType ( NXOpen.CAM.BoundaryTurnMemberFineFinishCornerValueType
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
BoundaryTurnMemberFineFinishCorner.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.