BoundaryTurnMemberFineFinishCornerValueType Enumeration

NXOpen.CAM.BoundaryTurnMemberFineFinishCorner.ValueType is an alias for NXOpen.CAM.BoundaryTurnMemberFineFinishCornerValueType

class NXOpen.CAM.BoundaryTurnMemberFineFinishCornerValueType

Bases: object

the corner types available

Enum Members

Enum Member Enum Member Description
General
AngularLine
TangentialLine
ShortenArcOrChamfer
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.