BoundaryTurnMemberFineFinishCornerAppliedTo Enumeration

NXOpen.CAM.BoundaryTurnMemberFineFinishCorner.AppliedTo is an alias for NXOpen.CAM.BoundaryTurnMemberFineFinishCornerAppliedTo

class NXOpen.CAM.BoundaryTurnMemberFineFinishCornerAppliedTo

Bases: object

the corner applied to available

Enum Members

Enum Member Enum Member Description
CurrentSegment
PreviousSegment
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.