BladeRough Class¶
-
class
NXOpen.CAM.
BladeRough
¶ Bases:
NXOpen.CAM.Blade
Represents a Blade Rough Drive Method Builder
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
BladeCleanupPasses | Returns or sets the blade cleanup passes |
CutDirection | Returns or sets the Cut Direction |
CutPattern | Returns the cut pattern builder |
CutStart | Returns the cut start location builder |
LeadingEdge | Returns the leading edge builder |
StartClosestToPreviousRetract | Returns or sets the Start Closest to Previous Retract |
Stepover | Returns the Stepover builder |
Tag | Returns the Tag for this object. |
TrailingEdge | Returns the trailing edge builder |
Methods¶
Property Detail¶
BladeCleanupPasses¶
-
BladeRough.
BladeCleanupPasses
¶ Returns or sets the blade cleanup passes
-------------------------------------
Getter Method
Signature
BladeCleanupPasses
Returns: the blade cleanup passes value value Return type: bool New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
BladeCleanupPasses
Parameters: bladeCleanupPasses (bool) – the blade cleanup passes value value New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
CutStart¶
-
BladeRough.
CutStart
¶ Returns the cut start location builder
-------------------------------------
Getter Method
Signature
CutStart
Returns: Return type: NXOpen.CAM.BladeCutStart
New in version NX7.5.0.
License requirements: None.
StartClosestToPreviousRetract¶
-
BladeRough.
StartClosestToPreviousRetract
¶ Returns or sets the Start Closest to Previous Retract
-------------------------------------
Getter Method
Signature
StartClosestToPreviousRetract
Returns: the Start Closest to Previous Retract value Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartClosestToPreviousRetract
Parameters: startClosestToPreRet (bool) – the Start Closest to Previous Retract value New in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
Stepover¶
-
BladeRough.
Stepover
¶ Returns the Stepover builder
-------------------------------------
Getter Method
Signature
Stepover
Returns: Return type: NXOpen.CAM.StepoverBuilder
New in version NX7.5.0.
License requirements: None.