Blade Class¶
-
class
NXOpen.CAM.
Blade
¶ Bases:
NXOpen.TaggedObject
Represents a Blade Rough Drive Method Builder
This is an abstract superclass that has instantaible subclasses
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
CutDirection | Returns or sets the Cut Direction |
CutPattern | Returns the cut pattern builder |
LeadingEdge | Returns the leading edge builder |
Tag | Returns the Tag for this object. |
TrailingEdge | Returns the trailing edge builder |
Methods¶
Enumerations¶
BladeMaterialSideType Enumeration | Available types for Flip Material, SDM: Select Cut Direction |
Property Detail¶
CutDirection¶
-
Blade.
CutDirection
¶ Returns or sets the Cut Direction
-------------------------------------
Getter Method
Signature
CutDirection
Returns: the Cut Direction value Return type: NXOpen.CAM.CutDirectionTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutDirection
Parameters: cutDirection ( NXOpen.CAM.CutDirectionTypes
) – the Cut Direction valueNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
CutPattern¶
-
Blade.
CutPattern
¶ Returns the cut pattern builder
-------------------------------------
Getter Method
Signature
CutPattern
Returns: Return type: NXOpen.CAM.CutPatternBuilder
New in version NX7.0.0.
License requirements: None.
LeadingEdge¶
-
Blade.
LeadingEdge
¶ Returns the leading edge builder
-------------------------------------
Getter Method
Signature
LeadingEdge
Returns: Return type: NXOpen.CAM.BladeEdge
New in version NX7.0.0.
License requirements: None.
TrailingEdge¶
-
Blade.
TrailingEdge
¶ Returns the trailing edge builder
-------------------------------------
Getter Method
Signature
TrailingEdge
Returns: Return type: NXOpen.CAM.BladeEdge
New in version NX7.0.0.
License requirements: None.