BladeCutStart Class¶
-
class
NXOpen.CAM.
BladeCutStart
¶ Bases:
NXOpen.TaggedObject
Represents a Blade Rough Drive Method Builder
This is an abstract superclass that has instantaible subclasses
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
From | Returns or sets the location of the cut start |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
BladeCutStartType Enumeration | Available types for Starting Cut |
Property Detail¶
From¶
-
BladeCutStart.
From
¶ Returns or sets the location of the cut start
-------------------------------------
Getter Method
Signature
From
Returns: location of cut start Return type: NXOpen.CAM.BladeCutStartType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
From
Parameters: startFrom ( NXOpen.CAM.BladeCutStartType
) – location of the cut startNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)