BladeCutStartType Enumeration

NXOpen.CAM.BladeCutStart.Type is an alias for NXOpen.CAM.BladeCutStartType

class NXOpen.CAM.BladeCutStartType

Bases: object

Available types for Starting Cut

Enum Members

Enum Member Enum Member Description
LeftOppositeRotaryaxis left opposite rotaryaxis
CenterOppositeRotaryaxis center opposite rotaryaxis
RightOppositeRotaryaxis right opposite rotaryaxis
LeftAlongRotaryaxis left along rotaryaxis
CenterAlongRotaryaxis center along rotaryaxis
RightAlongRotaryaxis right along rotaryaxis
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.