Graph Class¶
-
class
NXOpen.CAE.Xyplot.
Graph
¶ Bases:
NXOpen.CAE.Xyplot.BaseModel
Manages the display graph.
Each graph has its owner axis and graph name. Not support KF.
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
RecordCount | Returns the record count of the graph. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAssociativeMarker | Creates an associative marker. |
CreateAttributeIterator | Create an attribute iterator |
CreateMarker | Creates a marker in the position of a source point. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Find | Finds the NXObject with the given identifier as recorded in a journal. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAbscissaAxis | Gets the abscissa axis. |
GetAnchorPointOfRecord | Gets anchor point of a record. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetGridBoundingBox | Gets the bounding box of the grid. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMarkers | Gets all markers on the graph. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetOrdinateAxes | Gets the ordinate axes. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetPointCount | Gets the point count of specified record. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetRecordName | Gets record name. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetZAxis | Gets the Z axis. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDisplayStyleOfRecord | Sets the display style index for a plotted record. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unzoom | Removes the zoom state for the graph and returns the display to the original state. |
UpdateDisplay | Updates model display |
ZoomAlongX | Zooms the graph along X direction by a scale range basing on current X axis display range. |
ZoomAlongXY | Zooms the graph along both X and Y direction by scale ranges basing on current X and Y axis display range. It is only available to 2D plot. |
ZoomAlongY | Zooms the graph along Y direction by a scale range basing on current Y axis display range. |
ZoomAlongZ | Zooms the graph along Z direction by a scale range basing on current Z axis display range. It is only available to 3D plot. |
Property Detail¶
IsOccurrence¶
-
Graph.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Graph.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Graph.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Graph.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Graph.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Graph.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
CreateAssociativeMarker¶
-
Graph.
CreateAssociativeMarker
¶ Creates an associative marker.
The record index is between 0 and
CAE.Xyplot.Graph.RecordCount()
, 0 is inclusive.Signature
CreateAssociativeMarker(recordIndex, attachType, absPercentage)
Parameters: - recordIndex (int) – Record index
- attachType (
NXOpen.CAE.Xyplot.AnchorType
) – Attachment Type - absPercentage (float) – When attachment type is
CAE.XyplotAnchorType.AbsPercentage
, a valid abscissa percentage(between 0 and 1, both 0 and 1 are inclusive) should be given.
Returns: Marker model
Return type: New in version NX12.0.0.
License requirements: None.
CreateMarker¶
-
Graph.
CreateMarker
¶ Creates a marker in the position of a source point.
The record index is between 0 and
CAE.Xyplot.Graph.RecordCount()
, 0 is inclusive. The point index is between 0 andCAE.Xyplot.Graph.GetPointCount()
, 0 is inclusive.Signature
CreateMarker(recordIndex, pointIndex)
Parameters: - recordIndex (int) – Record index
- pointIndex (int) – Point index
Returns: Marker model
Return type: New in version NX10.0.0.
License requirements: None.
-------------------------------------
<summary> Creates a marker in the linear interpolation position between two source points. </summary>
The record index is between 0 and
CAE.Xyplot.Graph.RecordCount()
, 0 is inclusive. The previous point index is between 0 andCAE.Xyplot.Graph.GetPointCount()
, 0 is inclusive. The next point index is between 0 andCAE.Xyplot.Graph.GetPointCount()
, 0 is inclusive. The linear interpolation scale is between 0 and 1, both 0 and 1 are inclusive.Signature
CreateMarker(recordIndex, prePointIndex, nextPointIndex, linearInterpoScale)
Parameters: - recordIndex (int) – Record index
- prePointIndex (int) – Previous Point index
- nextPointIndex (int) – Next Point index
- linearInterpoScale (float) – Interpolation Scale
Returns: Marker model
Return type: New in version NX12.0.0.
License requirements: None.
-------------------------------------
Find¶
-
Graph.
Find
¶ Finds the
NXObject
with the given identifier as recorded in a journal. An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.An exception will be thrown if no object can be found with the given journal identifier.
Signature
Find(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX10.0.0.
Deprecated since version NX12.0.0: Use
NXOpen.INXObject.FindObject()
License requirements: None.
FindObject¶
-
Graph.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAbscissaAxis¶
-
Graph.
GetAbscissaAxis
¶ Gets the abscissa axis.
Signature
GetAbscissaAxis()
Returns: Return type: NXOpen.CAE.Xyplot.BasicModel
New in version NX11.0.0.
License requirements: None.
GetAnchorPointOfRecord¶
-
Graph.
GetAnchorPointOfRecord
¶ Gets anchor point of a record.
Signature
GetAnchorPointOfRecord(recordIndex, anchorType)
Parameters: - recordIndex (int) –
- anchorType (
NXOpen.CAE.Xyplot.AnchorType
) –
Returns: a tuple
Return type: A tuple consisting of (hasAnchorPoint, anchorPoint). hasAnchorPoint is a bool. anchorPoint is a
NXOpen.Point3d
.New in version NX11.0.0.
License requirements: None.
GetGridBoundingBox¶
-
Graph.
GetGridBoundingBox
¶ Gets the bounding box of the grid.
Signature
GetGridBoundingBox()
Returns: a tuple Return type: A tuple consisting of (leftBottom, rightTop). leftBottom is a NXOpen.Point3d
. rightTop is aNXOpen.Point3d
.New in version NX11.0.0.
License requirements: None.
GetMarkers¶
-
Graph.
GetMarkers
¶ Gets all markers on the graph.
Signature
GetMarkers()
Returns: Marker models Return type: list of NXOpen.CAE.Xyplot.MarkerModel
New in version NX10.0.0.
License requirements: None.
GetOrdinateAxes¶
-
Graph.
GetOrdinateAxes
¶ Gets the ordinate axes.
Signature
GetOrdinateAxes()
Returns: Return type: list of NXOpen.CAE.Xyplot.BasicModel
New in version NX11.0.0.
License requirements: None.
GetPointCount¶
-
Graph.
GetPointCount
¶ Gets the point count of specified record.
Signature
GetPointCount(recordIndex)
Parameters: recordIndex (int) – Record index Returns: Point count Return type: int New in version NX10.0.0.
License requirements: None.
GetRecordName¶
-
Graph.
GetRecordName
¶ Gets record name.
Signature
GetRecordName(recordIndex)
Parameters: recordIndex (int) – Returns: Return type: str New in version NX11.0.0.
License requirements: None.
GetZAxis¶
-
Graph.
GetZAxis
¶ Gets the Z axis.
Signature
GetZAxis()
Returns: Return type: NXOpen.CAE.Xyplot.BasicModel
New in version NX11.0.0.
License requirements: None.
Print¶
-
Graph.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetDisplayStyleOfRecord¶
-
Graph.
SetDisplayStyleOfRecord
¶ Sets the display style index for a plotted record.
The display style index is limitted from 0 to 19.
Signature
SetDisplayStyleOfRecord(recordIndex, displayStyleIndex)
Parameters: - recordIndex (int) –
- displayStyleIndex (int) –
New in version NX11.0.0.
License requirements: None.
SetName¶
-
Graph.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
Unzoom¶
-
Graph.
Unzoom
¶ Removes the zoom state for the graph and returns the display to the original state.
The function just updates the model data. To make the display update to reflect the model change, please call
CAE.Xyplot.BaseModel.UpdateDisplay()
for an instance ofCAE.Xyplot.Plot
orCAE.Xyplot.Graph
Signature
Unzoom()
New in version NX12.0.0.
License requirements: None.
UpdateDisplay¶
-
Graph.
UpdateDisplay
¶ Updates model display
Signature
UpdateDisplay()
New in version NX11.0.0.
License requirements: None.
ZoomAlongX¶
-
Graph.
ZoomAlongX
¶ Zooms the graph along X direction by a scale range basing on current X axis display range.
The function just updates the model data. To make the display update to reflect the model change, please call
CAE.Xyplot.BaseModel.UpdateDisplay()
for an instance ofCAE.Xyplot.Plot
orCAE.Xyplot.Graph
.The scale range could be calculated from
CAE.Xyplot.AxisModel.CalculateZoomScale()
Signature
ZoomAlongX(startScale, endScale)
Parameters: - startScale (float) – the value must be between 0 and 1
- endScale (float) – the value must be between 0 and 1
New in version NX12.0.0.
License requirements: None.
ZoomAlongXY¶
-
Graph.
ZoomAlongXY
¶ Zooms the graph along both X and Y direction by scale ranges basing on current X and Y axis display range. It is only available to 2D plot.
The function just updates the model data. To make the display update to reflect the model change, please call
CAE.Xyplot.BaseModel.UpdateDisplay()
for an instance ofCAE.Xyplot.Plot
orCAE.Xyplot.Graph
.The scale range could be calculated from
CAE.Xyplot.AxisModel.CalculateZoomScale()
Signature
ZoomAlongXY(xStartScale, xEndScale, yStartScale, yEndScale)
Parameters: - xStartScale (float) – the value must be between 0 and 1
- xEndScale (float) – the value must be between 0 and 1
- yStartScale (float) – the value must be between 0 and 1
- yEndScale (float) – the value must be between 0 and 1
New in version NX12.0.0.
License requirements: None.
ZoomAlongY¶
-
Graph.
ZoomAlongY
¶ Zooms the graph along Y direction by a scale range basing on current Y axis display range.
The function just updates the model data. To make the display update to reflect the model change, please call
CAE.Xyplot.BaseModel.UpdateDisplay()
for an instance ofCAE.Xyplot.Plot
orCAE.Xyplot.Graph
.The scale range could be calculated from
CAE.Xyplot.AxisModel.CalculateZoomScale()
Signature
ZoomAlongY(startScale, endScale)
Parameters: - startScale (float) – the value must be between 0 and 1
- endScale (float) – the value must be between 0 and 1
New in version NX12.0.0.
License requirements: None.
ZoomAlongZ¶
-
Graph.
ZoomAlongZ
¶ Zooms the graph along Z direction by a scale range basing on current Z axis display range. It is only available to 3D plot.
The function just updates the model data. To make the display update to reflect the model change, please call
CAE.Xyplot.BaseModel.UpdateDisplay()
for an instance ofCAE.Xyplot.Plot
orCAE.Xyplot.Graph
.The scale range could be calculated from
CAE.Xyplot.AxisModel.CalculateZoomScale()
Signature
ZoomAlongZ(startScale, endScale)
Parameters: - startScale (float) – the value must be between 0 and 1
- endScale (float) – the value must be between 0 and 1
New in version NX12.0.0.
License requirements: None.