AnchorType Enumeration¶
-
class
NXOpen.CAE.Xyplot.
AnchorType
¶ Bases:
object
Represents the anchor position of a record display, which is used to position a note Enum Members
Enum Member Enum Member Description NotSet the normal marker without anchor type Start the position of start point in a record display End the position of end point in a record display MaximumValue the position of the point which has maximum value in a record display MinimumValue the position of the point which has minimum value in a record display AbsPercentage the position of the point in the set abscissa percentage -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-