SolverAppendOption Class¶
-
class
NXOpen.CAE.
SolverAppendOption
¶ Bases:
NXOpen.NXObject
This class provides access to the append option setting for importing solver specific data into existing Fem/Sim
Not support KF.
New in version NX7.5.2.
Properties¶
Property | Description |
---|---|
CoordinateSystemOffset | Returns or sets the coordinate system offset |
DoAppendMerge | Returns or sets the append merge option |
ElementOffset | Returns or sets the element offset |
ImportBehavior | Returns or sets the import behavior choice |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MaterialMergeOption | Returns or sets the material merge choice |
Name | Returns the custom name of the object. |
NodeMergeOption | Returns or sets the node merge choice |
NodeOffset | Returns or sets the node offset |
OthersOffset | Returns or sets the offset for all other entities |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PhysicalPropertyOffset | Returns or sets the physical property offset |
PptMergeOption | Returns or sets the physical property merge choice |
Prototype | Returns the prototype of this object if it is an occurrence. |
SolutionMergeOption | Returns or sets the solution merge choice |
SolverName | Returns or sets the solver name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetHighestCoordinateSystemLabel | Gets the highest coordinate system label from the work Fem/Sim |
GetHighestElementLabel | Gets the highest element label from the work Fem/Sim |
GetHighestNodeLabel | Gets the highest node label from the work Fem/Sim |
GetHighestOthersLabel | Gets the highest label for all other entities from the work Fem/Sim |
GetHighestPhysicalPropertyLabel | Gets the highest physical property label from the work Fem/Sim |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
SolverAppendOptionImportBehaviorOption Enumeration | Options to control how the imported input file is to be combined with the existing model |
SolverAppendOptionMergeOption Enumeration | Options to control how entities are merge with existing model |
SolverAppendOptionSolutionOption Enumeration | Options to control if a solution is created during merge |
Property Detail¶
CoordinateSystemOffset¶
-
SolverAppendOption.
CoordinateSystemOffset
¶ Returns or sets the coordinate system offset
-------------------------------------
Getter Method
Signature
CoordinateSystemOffset
Returns: the coordinate system offset Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
CoordinateSystemOffset
Parameters: csOffset (int) – the coordinate system offset New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DoAppendMerge¶
-
SolverAppendOption.
DoAppendMerge
¶ Returns or sets the append merge option
-------------------------------------
Getter Method
Signature
DoAppendMerge
Returns: flag indicating if new entities should be merged with existing model Return type: bool New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAE.SolverAppendOption.ImportBehavior()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
DoAppendMerge
Parameters: doMerge (bool) – true if new entities should be merged with existing model New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.CAE.SolverAppendOption.SetImportBehavior()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ElementOffset¶
-
SolverAppendOption.
ElementOffset
¶ Returns or sets the element offset
-------------------------------------
Getter Method
Signature
ElementOffset
Returns: the element offset Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ElementOffset
Parameters: elemOffset (int) – the element offset New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ImportBehavior¶
-
SolverAppendOption.
ImportBehavior
¶ Returns or sets the import behavior choice
-------------------------------------
Getter Method
Signature
ImportBehavior
Returns: how the input file should be imported Return type: NXOpen.CAE.SolverAppendOptionImportBehaviorOption
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
ImportBehavior
Parameters: behaviorOption ( NXOpen.CAE.SolverAppendOptionImportBehaviorOption
) – how the input file should be importedNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
SolverAppendOption.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SolverAppendOption.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MaterialMergeOption¶
-
SolverAppendOption.
MaterialMergeOption
¶ Returns or sets the material merge choice
-------------------------------------
Getter Method
Signature
MaterialMergeOption
Returns: type of merging to perform for materials Return type: NXOpen.CAE.SolverAppendOptionMergeOption
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
MaterialMergeOption
Parameters: mergeChoice ( NXOpen.CAE.SolverAppendOptionMergeOption
) – type of merging to perform for materialsNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
SolverAppendOption.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
NodeMergeOption¶
-
SolverAppendOption.
NodeMergeOption
¶ Returns or sets the node merge choice
-------------------------------------
Getter Method
Signature
NodeMergeOption
Returns: type of merging to perform for nodes Return type: NXOpen.CAE.SolverAppendOptionMergeOption
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
NodeMergeOption
Parameters: mergeChoice ( NXOpen.CAE.SolverAppendOptionMergeOption
) – type of merging to perform for nodesNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
NodeOffset¶
-
SolverAppendOption.
NodeOffset
¶ Returns or sets the node offset
-------------------------------------
Getter Method
Signature
NodeOffset
Returns: the node offset Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
NodeOffset
Parameters: nodeOffset (int) – the node offset New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OthersOffset¶
-
SolverAppendOption.
OthersOffset
¶ Returns or sets the offset for all other entities
-------------------------------------
Getter Method
Signature
OthersOffset
Returns: the offset for all other entities Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
OthersOffset
Parameters: othersOffset (int) – the offset for all other entities New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OwningComponent¶
-
SolverAppendOption.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SolverAppendOption.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PhysicalPropertyOffset¶
-
SolverAppendOption.
PhysicalPropertyOffset
¶ Returns or sets the physical property offset
-------------------------------------
Getter Method
Signature
PhysicalPropertyOffset
Returns: the physical property offset Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
PhysicalPropertyOffset
Parameters: physicalPropertyOffset (int) – the physical property offset New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PptMergeOption¶
-
SolverAppendOption.
PptMergeOption
¶ Returns or sets the physical property merge choice
-------------------------------------
Getter Method
Signature
PptMergeOption
Returns: type of merging to perform for ppts Return type: NXOpen.CAE.SolverAppendOptionMergeOption
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
PptMergeOption
Parameters: mergeChoice ( NXOpen.CAE.SolverAppendOptionMergeOption
) – type of merging to perform for pptsNew in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Prototype¶
-
SolverAppendOption.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SolutionMergeOption¶
-
SolverAppendOption.
SolutionMergeOption
¶ Returns or sets the solution merge choice
-------------------------------------
Getter Method
Signature
SolutionMergeOption
Returns: type of merging to perform for solutions Return type: NXOpen.CAE.SolverAppendOptionSolutionOption
New in version NX9.0.0.
Deprecated since version NX10.0.0: Functionality moved to the solver language DLLs.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
SolutionMergeOption
Parameters: mergeChoice ( NXOpen.CAE.SolverAppendOptionSolutionOption
) – type of merging to perform for solutionsNew in version NX9.0.0.
Deprecated since version NX10.0.0: Functionality moved to the solver language DLLs.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SolverName¶
-
SolverAppendOption.
SolverName
¶ Returns or sets the solver name
-------------------------------------
Getter Method
Signature
SolverName
Returns: the solver name to indicate what type of data is being imported Return type: str New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Setter Method
Signature
SolverName
Parameters: solverName (str) – the solver name to indicate what type of data is being imported New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
FindObject¶
-
SolverAppendOption.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetHighestCoordinateSystemLabel¶
-
SolverAppendOption.
GetHighestCoordinateSystemLabel
¶ Gets the highest coordinate system label from the work Fem/Sim
Signature
GetHighestCoordinateSystemLabel()
Returns: the highest coordinate system label Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetHighestElementLabel¶
-
SolverAppendOption.
GetHighestElementLabel
¶ Gets the highest element label from the work Fem/Sim
Signature
GetHighestElementLabel()
Returns: the highest element label Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetHighestNodeLabel¶
-
SolverAppendOption.
GetHighestNodeLabel
¶ Gets the highest node label from the work Fem/Sim
Signature
GetHighestNodeLabel()
Returns: the highest node label Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetHighestOthersLabel¶
-
SolverAppendOption.
GetHighestOthersLabel
¶ Gets the highest label for all other entities from the work Fem/Sim
Signature
GetHighestOthersLabel()
Returns: the highest label for all other entities Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetHighestPhysicalPropertyLabel¶
-
SolverAppendOption.
GetHighestPhysicalPropertyLabel
¶ Gets the highest physical property label from the work Fem/Sim
Signature
GetHighestPhysicalPropertyLabel()
Returns: the highest physical property label Return type: int New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Print¶
-
SolverAppendOption.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SolverAppendOption.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.