SolverAppendOptionImportBehaviorOption Enumeration

NXOpen.CAE.SolverAppendOption.ImportBehaviorOption is an alias for NXOpen.CAE.SolverAppendOptionImportBehaviorOption

class NXOpen.CAE.SolverAppendOptionImportBehaviorOption

Bases: object

Options to control how the imported input file is to be combined with the existing model

Enum Members

Enum Member Enum Member Description
AppendModel
MergeWithExisting
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.