SelectionRecipe Class¶
-
class
NXOpen.CAE.
SelectionRecipe
¶ Bases:
NXOpen.DisplayableObject
Represents a class
NXOpen.CAE.SelectionRecipe
.This is an abstract class
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
IsBlanked | Returns the blank status of this object. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Display | Returns the display attributes belonging to the Selection Recipe |
Methods¶
Method | Description |
---|---|
Blank | Blanks the object. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetEntities | Gets entities in the Selection Recipe. |
GetEntityTypes | Returns Entity Types supported by the Selection Recipe. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetName | Gets the name of the Selection Recipe |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasNonDisplayableEntities | Returns whether the Selection Recipe has non-displayable entities |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
HideContents | Hide the contents of the Selection Recipe. |
Highlight | Highlights the object. |
Information | Display information of this Selection Recipe |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the name of the Selection Recipe |
SetNameLocation | Sets the location of the object’s name. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
ShowContents | Show the contents of the Selection Recipe. |
ShowContentsOnly | Shows the contents of the Selection Recipe only. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
Property Detail¶
IsOccurrence¶
-
SelectionRecipe.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SelectionRecipe.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SelectionRecipe.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SelectionRecipe.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SelectionRecipe.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SelectionRecipe.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Display¶
-
SelectionRecipe.
Display
¶ Returns the display attributes belonging to the Selection Recipe
Signature
Display
New in version NX12.0.0.
Returns: Return type: NXOpen.CAE.SelectionRecipeDisplay
Method Detail¶
FindObject¶
-
SelectionRecipe.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetEntities¶
-
SelectionRecipe.
GetEntities
¶ Gets entities in the Selection Recipe.
Signature
GetEntities()
Returns: Return type: list of NXOpen.TaggedObject
New in version NX12.0.0.
License requirements: None.
GetEntityTypes¶
-
SelectionRecipe.
GetEntityTypes
¶ Returns Entity Types supported by the Selection Recipe.
Signature
GetEntityTypes()
Returns: Entity types to which this recipe resolves to. Return type: list of NXOpen.CAE.CaeSetGroupFilterType
New in version NX12.0.0.
License requirements: None.
GetName¶
-
SelectionRecipe.
GetName
¶ Gets the name of the Selection Recipe
Signature
GetName()
Returns: Return type: str New in version NX12.0.0.
License requirements: None.
HasNonDisplayableEntities¶
-
SelectionRecipe.
HasNonDisplayableEntities
¶ Returns whether the Selection Recipe has non-displayable entities
Signature
HasNonDisplayableEntities()
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
HideContents¶
-
SelectionRecipe.
HideContents
¶ Hide the contents of the Selection Recipe.
Note that
CAE.FEElemEdge
,CAE.FEElemFace
andCAE.CAEEdge
do not participate in this command. They are non-displayable entities and are never drawn individually in NX. UseNXOpen.CAE.SelectionRecipe.HasNonDisplayableEntities()
to determine if the Selection Recipe contains these entities.Signature
HideContents()
New in version NX12.0.0.
License requirements: None.
Information¶
-
SelectionRecipe.
Information
¶ Display information of this Selection Recipe
Signature
Information()
New in version NX12.0.0.
License requirements: None.
Print¶
-
SelectionRecipe.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SelectionRecipe.
SetName
¶ Sets the name of the Selection Recipe
Signature
SetName(name)
Parameters: name (str) – New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ShowContents¶
-
SelectionRecipe.
ShowContents
¶ Show the contents of the Selection Recipe.
Note that
CAE.FEElemEdge
,CAE.FEElemFace
andCAE.CAEEdge
do not participate in this command. They are non-displayable entities and are never drawn individually in NX. UseNXOpen.CAE.SelectionRecipe.HasNonDisplayableEntities()
to determine if the Selection Recipe contains these entities.Signature
ShowContents()
New in version NX12.0.0.
License requirements: None.
ShowContentsOnly¶
-
SelectionRecipe.
ShowContentsOnly
¶ Shows the contents of the Selection Recipe only.
Note that
CAE.FEElemEdge
,CAE.FEElemFace
andCAE.CAEEdge
do not participate in this command. They are non-displayable entities and are never drawn individually in NX. UseNXOpen.CAE.SelectionRecipe.HasNonDisplayableEntities()
to determine if the Selection Recipe contains these entities.Signature
ShowContentsOnly()
New in version NX12.0.0.
License requirements: None.