ResultMeasureResultDirectionOptions Class¶
-
class
NXOpen.CAE.
ResultMeasureResultDirectionOptions
¶ Bases:
NXOpen.CAE.ResultMeasureResultOptions
Represents the result directional options for result measure
To obtain an instance of this class use
CAE.ResultMeasureCollection
.New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
SetAbsoluteValue | Set the option to use absolute values |
SetCoordinateSystem | Set the coordinate system for directional components |
SetOperation | Set the operation type |
SetPlynum | Set the ply num in result option |
SetUnit | Set the unit |
Method Detail¶
Dispose¶
-
ResultMeasureResultDirectionOptions.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
SetCoordinateSystem¶
-
ResultMeasureResultDirectionOptions.
SetCoordinateSystem
¶ Set the coordinate system for directional components
Signature
SetCoordinateSystem(eCsys)
Parameters: eCsys ( NXOpen.CAE.ResultCoordinateSystem
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)