StrainGageBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
StrainGageBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.BaseBuilder
Represents a StrainGageBuilder
To create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.StrainGageCollection.CreateStrainGageBuilder()
Default values.
Property Value GageType UniAxial Placement Node Plane FacePlane ResultType Strain RotationAngle.Value 0.0 (millimeters part), 0.0 (inches part) ShellElementFace Top New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Csys | Returns or sets the orientation direction, Only available when the strain gage’s orientation plane type is CAE.ResponseSimulationStrainGageOrientationPlane.Csys |
GageType | Returns or sets the type of strain gage |
ObjectLabel | Returns the object label |
Placement | Returns or sets the placement type of strain gage |
Plane | Returns or sets the orientation plane type of strain gage |
ResultType | Returns or sets the result type of strain gage |
RotationAngle | Returns the rotation angle, Only available when the strain gage’s orientation plane type is CAE.ResponseSimulationStrainGageOrientationPlane.Csys |
SelectedElementFaces | Returns the selected element face. |
SelectedNode | Returns the destination nodes, Only available when the strain gage’s placement type is CAE.ResponseSimulationStrainGagePlacementType.Node |
ShellElementFace | Returns or sets the shell element face location type of strain gage |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Csys¶
-
StrainGageBuilder.
Csys
¶ Returns or sets the orientation direction, Only available when the strain gage’s orientation plane type is
CAE.ResponseSimulationStrainGageOrientationPlane.Csys
-------------------------------------
Getter Method
Signature
Csys
Returns: Return type: NXOpen.SmartObject
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
Csys
Parameters: orientationCoordSystem ( NXOpen.SmartObject
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GageType¶
-
StrainGageBuilder.
GageType
¶ Returns or sets the type of strain gage
-------------------------------------
Getter Method
Signature
GageType
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrainGageType
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
GageType
Parameters: gageType ( NXOpen.CAE.ResponseSimulation.StrainGageType
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Placement¶
-
StrainGageBuilder.
Placement
¶ Returns or sets the placement type of strain gage
-------------------------------------
Getter Method
Signature
Placement
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrainGagePlacementType
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
Placement
Parameters: gagePlacement ( NXOpen.CAE.ResponseSimulation.StrainGagePlacementType
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Plane¶
-
StrainGageBuilder.
Plane
¶ Returns or sets the orientation plane type of strain gage
-------------------------------------
Getter Method
Signature
Plane
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrainGageOrientationPlane
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
Plane
Parameters: plane ( NXOpen.CAE.ResponseSimulation.StrainGageOrientationPlane
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ResultType¶
-
StrainGageBuilder.
ResultType
¶ Returns or sets the result type of strain gage
-------------------------------------
Getter Method
Signature
ResultType
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrainGageResult
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ResultType
Parameters: resultType ( NXOpen.CAE.ResponseSimulation.StrainGageResult
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
RotationAngle¶
-
StrainGageBuilder.
RotationAngle
¶ Returns the rotation angle, Only available when the strain gage’s orientation plane type is
CAE.ResponseSimulationStrainGageOrientationPlane.Csys
-------------------------------------
Getter Method
Signature
RotationAngle
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SelectedElementFaces¶
-
StrainGageBuilder.
SelectedElementFaces
¶ Returns the selected element face.
Only available when the strain gage’s placement type is
CAE.ResponseSimulationStrainGagePlacementType.ElementFaceCenter
-------------------------------------
Getter Method
Signature
SelectedElementFaces
Returns: Return type: NXOpen.CAE.SelectFEElemFaceList
New in version NX7.5.2.
License requirements: nx_response_anlys (“NX Response Analysis”)
SelectedNode¶
-
StrainGageBuilder.
SelectedNode
¶ Returns the destination nodes, Only available when the strain gage’s placement type is
CAE.ResponseSimulationStrainGagePlacementType.Node
-------------------------------------
Getter Method
Signature
SelectedNode
Returns: Return type: NXOpen.CAE.SelectFENodeList
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ShellElementFace¶
-
StrainGageBuilder.
ShellElementFace
¶ Returns or sets the shell element face location type of strain gage
-------------------------------------
Getter Method
Signature
ShellElementFace
Returns: Return type: NXOpen.CAE.ResponseSimulation.StrainGageShellElementFaceType
New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ShellElementFace
Parameters: shellElementFace ( NXOpen.CAE.ResponseSimulation.StrainGageShellElementFaceType
) –New in version NX6.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
Validate¶
-
StrainGageBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.